cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 - MPU Configuration

yilmazkircicek
Associate III

Hi All, 

I was testing my new STM32H746XIH6 board and met the post below by @GSpre.1 during a search about SDRAM  performance. 

GSpre.1 - Performance characteristics of SDRAM on STM32F7508-DISCO board 

I don't have a lot of time to read MPU documentation, maybe someone has an idea about the code piece below that @GSpre.1  adviced. 

 

I did not perform a precise measurement but used Systick for both internal and external (32-bit SDRAM) memory array manipulation time for the same data length. (I-Cache and D-Cache are both enabled as expected.)

Internal memory test:  12ms 

External memory test: 47ms without the code below  

External memory test: 13ms.with the code below

 

* What exactly the code below does ? 

* Am I compromising from anything for speed ? 

 

There are a lot of job to do during board bring-up I have no time to read a lot of documentation. I will be appreciated if someone share experience...

BTW, thanks for sharing @GSpre.1

Regars. 

 

MPU_Region_InitTypeDef MPU_InitStruct; HAL_MPU_Disable(); MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.BaseAddress = 0xD0000000; MPU_InitStruct.Size = MPU_REGION_SIZE_32MB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

 

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Hello,

The address 0xDXXX XXXX is not a cacheable region by default. Device means not cacheable even the caches are enabled (data and instruction).

mALLEm_0-1742740114256.png

The code you shared makes the 0xDXXX XXXX region cacheable.

So the results you shared are expected.

Hope that helps

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mÆŽALLEm
ST Employee

Hello,

The address 0xDXXX XXXX is not a cacheable region by default. Device means not cacheable even the caches are enabled (data and instruction).

mALLEm_0-1742740114256.png

The code you shared makes the 0xDXXX XXXX region cacheable.

So the results you shared are expected.

Hope that helps

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Dear @mÆŽALLEm ,

I thank you for your prompt response, especially on Sunday :) 

Regards.