2024-11-19 07:14 PM
After STM32H5 I3C initialized as a controller, without any IBI, HotJoin Enabled, pull low SDA line will case SCL unstopped-toggle, as figure
I had searched STM32H563 Errata 2.5.13, and got something likes this behavior :
I3C controller: unexpected first frame with a 0x7F address when the I3C peripheral is enabled
Description
After I3C has been initialized as controller, an unexpected frame is generated when the I3C peripheral is enabled.
The issue occurs after the following sequence:
1. I3C is initialized as I3C controller (CRINIT bit is set in I3C_CFGR whereas EN bit is kept cleared in
I3C_CFGR).
2. I3C is enabled (EN bit set in I3C_CFGR).
As a result, the I3C controller can incorrectly detect that the SDA line has been driven low by a target, interpret it
as a start request, activate the SCL clock, and generate a 0x7F address followed by RNW bit = 1 that is not
acknowledged.
This first frame completes without any other impact than this unexpected I3C bus activity.
Workaround
Respect the sequence below during I3C controller initialization:
1. Instead of configuring the alternate GPIO of the SDA line without any pull-up, temporary enable the GPIO pullup.
2. After a delay of 1 ms, disable GPIO pull-up.
3. Initialize I3C as I3C controller by setting CRINIT in I3C_CFGR whereas EN bit is kept cleared in I3C_CFGR.
4. Enable I3C by setting EN bit in I3C_CFGR.
As a result the I3C controller does not detect SDA low when it is enabled, and no unexpected frame is generated
**Question**
I had followed the errata solution, but the problem is still not solved,
Do you have any idea?
Here is my code :
I3C1->CFGR &= ~(I3C_CFGR_EN | I3C_CFGR_CRINIT);
LL_GPIO_SetPinPull(GPIOB, LL_GPIO_PIN_9, LL_GPIO_PULL_UP);
HAL_Delay(1);
LL_GPIO_SetPinPull(GPIOB, LL_GPIO_PIN_9, LL_GPIO_PULL_NO);
I3C1->CFGR |= I3C_CFGR_CRINIT;
I3C1->CFGR |= I3C_CFGR_EN ;
2025-01-07 05:19 AM
Hello @SUPA786 ,
First of all, could you please specify your HW setup?
Then, the I3C controller parameters .
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-07 05:15 PM
Hello, @Foued_KH , thanks for your reply,
I am using demo board [NUCLEOH-563ZI] for my Hardware without connect any slave device,
I keep pin PB8(I3C1_SCL), PB9(I3C1_SDA) floating when power up, and then pull SDA to GND cause SCL unstopped-toggle, as figure above
In Legacy I2C Bus scenario, there is other Host I2C share the bus, it might be a problem.
Here is my I3C initial code :
2025-01-08 01:46 AM
Hello @SUPA786 ,
If you disable the IBI and HotJoin as well, you will not see this behavior.
My recommendation is to connect an I3C target on the bus :
When using a sensor as an I3C target, you need to check the maximum frequency for the communication.
If you are using another STM32H5 MCU as an I3C target, you can communicate at 12.5 MHz.
Let me know if this helps you!
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-08 07:14 PM
Hello, @Foued_KH
If you disable the IBI and HotJoin as well, you will not see this behavior.
I think I am not enabled either IBI or HotJoin, here is my I3C registers after initilized, did I miss something?
My recommendation is to connect an I3C target on the bus :
I am developing a I3C-adaptor , a tool of I3C, so I can't not decide the which target will be connected to the bus
thanks for your reply
Yours Sincerely.