cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 I3C SDR READ issue

wulin
Associate

Hello, when I was using the STM32H563 I3C, I found that when configured with VDDIO2 = 1.2V and a frequency of 12.5MHz, the data read in SDR mode would be misaligned. The waveform received on the SDA line was 0xF9, but the MCU received 0x7C. After I increased the VDDIO voltage to 1.5V, the data read was correct. And I tried VDDIO2=1.2V, frequency =6.25Mhz, data was correct, too.

wulin_0-1737098779073.png

 

wulin_2-1737098807751.png

 

2 REPLIES 2
mƎALLEm
ST Employee

Hello @wulin and welcome to the community,

It could be something related to the HSLV configuration. Refer to the datasheet / and tables:

Output timing characteristics VDDIO2 1.2 V range (HSLV OFF)

Output timing characteristics VDDIO2 1.2 V (HSLV ON)

Did you activate the HSLV?

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello, @mƎALLEm , thank you for your reply.

HSLV was disabled in my previous setting. But I tried to set HSLV ON, the result was still the same as before.

wulin_0-1737361089357.png