cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 DA Discover error: Failed to communicate with target

adrianpop
Visitor

Hi, 

 

I'm just starting to play with a NUCLEO-H563ZI and I have some problems with DA discover using my dev boards.

I started to do the following steps: 

Step 1: Create the provisioning file (.obk file)
--> STM32TrustedPackageCreator_CLI.exe --obk H5\Config\DA_ConfigWithPassword.xml

Step 2: Program the application binary
-->STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -d H5\Binary\MyProject.elf -v

Step 3: Move to the PROVISIONING state.
--> STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob PRODUCT_STATE=0x17

Step 4: Provisioning the .obk file
--> STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -sdp H5\Binary\DA_ConfigWithPassword.obk

And after these steps I just tried the following command:

--> STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG debugauth=2

but here I received the following error: 

adrianpop_0-1733301099969.png

When I saw this I open STM32CubeProgrammer in order to made a DA discover from there but I received also from there an error: 

adrianpop_1-1733301155233.png

In this step from what I saw I'm able to made a connection between STM32CubeProgrammer and my dev boars only if I will use "HotPlug" mode.

For testing purpose I tried to revert the PRODUCT_STATE to 0xED but I received the following error: 

adrianpop_2-1733301339532.png

Do you have any idea how can I recover my board ? 

Thanks in advance!

Adrian Pop

 

0 REPLIES 0