cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G431CBU6 has UART4 !

mwalt.3
Associate III
Hi, 
as advertised
of course , but no :
- no UART4 as the datasheet , page 14/200 (false because UFQFPN48 has 4 more pins than LQFP48 ?)
- no UART4 as CubeMx : PC10 and PC11 are present , but no UART4
I have got a STM32G431CBU6 from an chinese board maker , nice board with amazing MCU
tried UART4 as STM32duino's Serial4 : it works , so USART4 is present , officially or not ...
(didn't try the handshaking lines)
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @mwalt.3 ,

The issue is fixed in DS12589 Rev 6 and in STM32CubeMX 6.11.0.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
AScha.3
Chief III

as page 14 shows, STM32G431CBU6 should have the uart, only in lqfp48 not.

(lqfp48 has more vdd/vss pins, so pc10/11 missing)

AScha3_0-1688281791502.png

 

If you feel a post has answered your question, please click "Accept as Solution".
oh right , thanks , I had (don't now why) Rev 2 , but its actually Rev 6
still the issue with CubeMx
KDJEM.1
ST Employee

Hello @mwalt.3 ,

I confirm this issue in the STM32CubeMX 6.8.1 version.

I reported this issue internally. 

Internal ticket number: 146117 (This is an internal tracking number and is not accessible or usable by customers).

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hello @mwalt.3 ,

The issue is fixed in DS12589 Rev 6 and in STM32CubeMX 6.11.0.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.