2026-05-05 8:10 AM - last edited on 2026-05-05 10:00 AM by mƎALLEm
Hello,
in an earlier post it was suggested to reset the FDCAN for full error recovery using RCC_APBRSTR1.FDCANRST Bit
This bit seems to be global for all FDCAN instances.
Is it correct that full error recovery in one FDCAN instance is not possible without interrupting traffic in the other instance - as all (or both in case of stm32g0b1) instances have to be reset?
t
2026-05-05 10:00 AM
Hello,
Do you mean a recovery from Bus-Off state?
This is How to recover from Bus-Off state with FDCAN on STM32 MCUs without performing a reset of the peripheral.