2021-08-10 2:36 PM
Hi, I've been working with this device for a while.
Today I started to try to write the option bytes in order to turn PF2 into a GPIO, which I did by writing an assembly file, compiling, and flashing via debug in Keil. I use a Segger J-Link as USB SWD interface
At one point Keil informs that it can't perform mass erase (which have been doing for quite a while). I connect with Segger Flash, which informs there is a protection in place and asked to perform mass erase, which resulted in an error I can't recall.
After that, the device is not detected by Keil, it doesn't show up as a connected device as before and Segger Flash can't connect to it.
Anything I can try ?
What could have caused this ? I wonder if Segger could have tried a "manual mass erase" and set BOOT_LOCK. As I said, have been mass erasing with Keil for a long time while working on this project.
Thanks
2021-08-20 3:14 AM
Hi @scaprile ,
Is it possible for you to check with STM32CubeProgrammer?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-08-20 8:32 AM
Since that tool does not support the Segger J-Link, and I don't own an ST-Link, I can only try connecting via the bootloader on the UART, what I already tried with stm32loader (https://github.com/florisla/stm32loader), to same result: no connection.