cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0 not works after reset

Samira Foroughi
Associate II

Hello

I work on the stm32g0 micro.

i programmed it with a simple "blinky" code.

it works correctly.but when i reset it doesn't work until i program it again.

can you help me?

14 REPLIES 14
Samira Foroughi
Associate II

hello

I bought a standard test board, and tested with it, the problem still exists.

KnarfB
Principal III

What chip/board are you exactly using?

JCuna.1
Senior

The same problem for me and the year is almost gone. When ST pretend to solve this problem?

Ok, I got a workaround, changing bit nboot_sel from 1 to 0 fix the problem of bad reset while debugging.0693W00000GYWH6QAP.png

S.Ma
Principal

This is because G0 goes down to small pincount packages, hence Reset can be gpio, boot pin is also swd signal for debug.