2019-12-15 06:18 PM
Hi, I'm just a Firmware Engineer
recently, i 've designed the mcu circuits.
i 've checked the stm32f072 DISCOVERY Board few days ago.
in the board block, it embedded SWD (2-Wire for J-TAG)
--------------------------------------------------------------------------------------------------------
USB Connector --- MCU(STM32F103) for SWD --- MAIN MCU (STM32F072)
--------------------------------------------------------------------------------------------------------
so, i decided to embed it.
but i have some curious...
how could i get SWD firmware??
because the circuits for SWD and interface logic is provided by ST, it is not difficult to design it
but, i think the MCU for SWD is also needed for some firmware which is operating SWD (J-TAG)
does anyone know this? or am i stupid?
2019-12-15 08:57 PM
ST doesn't provide the firmware, but it can be found with a Google search
2019-12-15 09:07 PM
thank you for your comment!
2019-12-16 12:26 AM
For next design, you may also want to consider to use the ready-to-solder STLINK-V3MODS module instead.