2023-06-26 01:48 AM
Hi,
I am using a STM32F767zi nucleo board as SPI full duplex slave. The dummy cycles of the slave device is varies in accordance with the master frequency change. How can I handle the dummy cycles independent of master frequency? What is the solution for making fixed dummy cycles for various master frequencies?
Thanks and regards,
Arjun
2023-06-26 02:23 AM
you set: SPI full duplex slave , so all clock/cycles coming from master, you cannot change any clock on slave side.
you need to change at master.
2023-06-26 02:33 AM
I don't need to change the frequency from the slave side, I have to make the dummy cycles needed for the slave independent of input master frequency.