2018-05-29 11:34 PM
Hello friends,
I try SPI communication, and I have a problem. I only send data.... But how to receive it?
Connection is:
1. one master - one slave
2. Full duplex
Initialize:
LL_SPI_InitTypeDef SPI_InitStruct;
LL_GPIO_InitTypeDef GPIO_InitStruct;LL_SPI_Disable(SPI1);
LL_AHB1_GRP1_EnableClockLL_AHB1_GRP1_PERIPH_GPIOA);
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
/* SPI2 GPIO Configuration */
GPIO_InitStruct.Pin = LL_GPIO_PIN_5; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_7; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_6; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_4; GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; GPIO_InitStruct.Alternate = LL_GPIO_AF_5; LL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* SPI1 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX; SPI_InitStruct.Mode = LL_SPI_MODE_MASTER; SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT; SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_HIGH; SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE; SPI_InitStruct.NSS = LL_SPI_NSS_HARD_OUTPUT; SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV64; SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST; SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE; SPI_InitStruct.CRCPoly = 7; LL_SPI_Init(SPI1, &SPI_InitStruct);LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_EnableNSSPulseMgt(SPI1);LL_SPI_SetRxFIFOThreshold(SPI1, LL_SPI_RX_FIFO_TH_QUARTER);
/* Configure SPI1 transfer interrupts */
/* Enable RXNE Interrupt */ LL_SPI_EnableIT_RXNE(SPI1);LL_SPI_Enable(SPI1);
And function to write/read....
int32_t read_from_reg(SPI_TypeDef *SPI, uint8_t data, uint8_t *SPI_Data_receive)
{ LL_SPI_TransmitData8(SPI, data); while (!LL_SPI_IsActiveFlag_TXE(SPI)); while (!LL_SPI_IsActiveFlag_RXNE(SPI)); while (LL_SPI_IsActiveFlag_BSY(SPI)); *SPI_Data_receive = LL_SPI_ReceiveData8(SPI);return 0;
}And I sent one byte and I don't receive anything. Any idea, how to receive some data from register?
#nucleo-f767zi #stm32f7-spi Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-05-30 06:14 AM
Strange that the code shows initialisation with HARD_OUTPUT (the code must enable SSOE) and registers tell that SSI+SSM are one whereas they should be zero. Are you sure to run the right code ?
2018-05-30 06:17 AM
I modification my code to control NSS pin by software:
GPIO_InitStruct.Pin = LL_GPIO_PIN_4;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT; GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; LL_GPIO_Init(GPIOA, &GPIO_InitStruct);and here is my log scope, where I send 3 dummy and read 3 bytes....
:)
Now, it is work, but ......2018-05-30 06:25 AM
A modif the function to use : LL_SPI_NSS_HARD_OUTPUT
And now egister is set:
SSOE = 0x01
SSI = 0x01
SSM = 0x00
2018-05-30 06:37 AM
SR
every 8 clock cycles the Rx register will have the value of the MISO pins.
and RXNE is set.
2018-05-30 06:41 AM
Well, the SPI has 4 words FIFO, so that you can write 4 times to DR in a row and the SPI shall generate the correct waveform with CE down for the duration of 4 time 8-bit characters. Can you observe that ? Then manage your reception.
2018-05-30 06:50 AM
Some peripherals like the nSS to be active between bytes,
But others like it to run over the whole command.
where is the nSS line trace ?
2018-05-30 07:04 AM
:)
NSS = CE on my picture.2018-05-30 10:41 AM
Can you see that nSS is not high then going low to start the command.
you need nSS to be high on startup.
2018-05-31 04:00 AM
If the same simple program works when PA15 is used as NSS, but not if PA4 is used as NSS, then it's time to talk to ST's support...
JW
2018-05-31 08:16 AM
I reconnected it back to PA4 and it's working.
Because my first test function was without LL_SPI_Enable/LL_SPI_Disable.