2019-07-04 1:48 AM
2019-07-04 4:15 AM
AFAIK, no.
It is designed so that two QSPI memories can be connected, but they are accessed simultaneously, mimicking 8-bit access.
JW
2019-07-04 4:22 AM
Hi JW
Thanks for answering
So as i understood the QSPI interface is for memory only ?
Or i can connect one slave device (like FPGA) instead of memory ?
2019-07-04 4:29 AM
My understanding is that it can be used in an interleaving mode, but also has two distinct bank pins allowing for different memory types. If the manuals are not clear on this, discuss with an FAE.
I'd expect an FPGA could be used in the same way as a QSPI RAM device.