2017-08-15 2:28 PM
1. ST-Link reports the wrong size for the Flash memory. ST-LINK-Utility reports 'Unknown' and the ST-Link CLI reports 4095 kBytes.
2. ST-Link CLI can't erase memory sector 1 at 0x08004000. When using the commandline-switch -SE 0 1 st-link cli reports the following Error:
Memory Sector @0x8000000 erased
Memory Sector @0x8004000 is not erased. Verify the memory protection.
Verifying the Option-Bytes the memory is not protected!!!
Only a full chip erase can resolve this problem.
Solved! Go to Solution.
2017-08-22 1:59 PM
A new version of ST-Link software is online. The STM32F723-bug is fixed. Thank you.
2017-08-16 1:25 AM
Hi
Reuss.Erwin
,Are you using the last version of STLink Utility?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-08-16 9:42 AM
Yes of course. I am always using the latest version from the ST homepage. ST-Link Utility v4.0.0.0, STLinkUSBDriver.dll v4.4.0.0 and ST-LINK_CLI.exe v3.0.0.0.
All works perfect, wenn i do a full erase before flashing. But this always takes a long time.
2017-08-22 1:59 PM
A new version of ST-Link software is online. The STM32F723-bug is fixed. Thank you.
2017-08-22 7:53 PM
V4.1.0
http://www.st.com/en/embedded-software/stsw-link004.html