2022-10-12 2:41 AM
Hi.
I`m going to use an octal uart IC named XR16V798 and my MCU is a stm32f756z,
I printed my own designed board which connected these two ICs as follows:
just to mention, I haven`t used FMC with any other device before, now I dont know how to work with this IC,
stm32cubemx version 6.5.0 generated the code.
thanks.
2022-10-12 5:26 AM
Read the FMC chapter in RM.
Your chip's registers are now mapped to STM32's memory, as you use FMC_NE1 ie. Bank 1 - NOR/PSRAM 1, at address 0x6000'0000. It means, you can access the registers e.g. in this way:
#define XR16V798_REG0 *(volatile uint8_t*)0x60000000
#define XR16V798_REG1 *(volatile uint8_t*)0x60000001
XR16V798_REG0 = new_value_for_register_0;
readout_value_from_register_1 = XR16V798_REG1;
However, to get this working properly in 'F7, you need to set the region starting at 0x6000'0000 as Device in MPU. Alternatively, remap it to 0xC000'0000 using SYSCFG_MEMRMP.SWP_FMC, then the above macros would of course also using the 0xC0000000 address.
JW
2022-10-15 6:21 AM
Thanks for reply.
Definitely was not going to work without these helps you put here, is there any comprehensive application note that I can use to setup these registers? there is no good source for that.
thanks again.
2022-10-16 12:45 AM
Probably not a single concise document, so you have to go through all available materials, i.e. the Cortex-M7 UM, the DS/RM/ES combination, and selected application notes such as AN4838/AN4839. You can also check out the "tips" section in AN4891, while that's for 'H7 some of the tips pertain to 'F7 too.
JW
2022-10-16 4:44 AM
That was a really hard job. I added some piece of code as you mentioned:
in header file
#define MPU_TYPE (*((volatile unsigned long*) 0xE000ED90))
#define MPU_CTRL (*((volatile unsigned long*) 0xE000ED94))
#define MPU_RNR (*((volatile unsigned long*) 0xE000ED98))
#define MPU_RBAR (*((volatile unsigned long*) 0xE000ED9C))
#define MPU_RASR (*((volatile unsigned long*) 0xE000EDA0))
in C file
void Config_MPU(void)
{
MPU_RNR = 0x00000003;
MPU_RBAR = 0x60000000;
MPU_RASR = 0x0301FF0F;
MPU_CTRL = 0x00000005;
}
and after those in my main file, I have:
SYSCFG->MEMRMP &= 0xfffff3ff;
SYSCFG->MEMRMP |= 1<<10;
not any success. I cant see any square waves in my oscope.
Thanks for the help.