cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 DCMI_DR always zero

ferhatyol-23
Senior
Posted on February 10, 2016 at 12:21

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
5 REPLIES 5
ferhatyol-23
Senior
Posted on February 11, 2016 at 10:53

hi all

Do you have any idea? What could be the problem?

Avner Gidron
Associate II
Posted on June 18, 2017 at 07:14

Hi,

I have the same problem in my STM32F769 eval. Have you figured it out? in my case I see that the DMA gets FIFO error. Is that the case tou have?

Thanks,

Avner

wang dobby
Associate
Posted on March 07, 2018 at 09:28

Hi,

I think you may have fixed the issue, right?

Unfortunately, I am using ov9655 and STM32H743Zi Nucleo board and trying to capture pictures. But I have the similar issue now, I can get only 0x00 data from DCMI_DR, even if Vsync, Hsync, frame interrupts works, and it seems data with 

logic analyzer on D0~D7.

Can you please help to introduce how did you fix it in your side? Thanks in advance and hope your feedback soon.

Regarsds

Dobby

Roberto Fratta
Associate II
Posted on June 29, 2018 at 10:14

Hi all,

Same issue for me, someone has solved?

Posted on June 29, 2018 at 12:52

Hello All,

I recommend to check the GPIO configuration, as well as the DCMI.

Also, check all control signals: PIXCLK, HSYNC and VSYNC.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen