2017-04-11 7:03 AM
Hi,
I'm facing an issue with a new project I'm working on, I just received a custom board based on a STM32F746VGT6 MCU, the MCU wasn't able to run my base program, (generated via MXCube), so I started changing parameters to find the source, and it led me to this : when I bring the clock speed down my program run without problems. But when I run with frequencies above ~120MHz, then the program stop working. For now my program just toggle 2 GPIOs : one in the systick handler and the other in a timer interrupt.
At first I thought it could be a problem between openocd and the board, but even without the debugger the program wont run above 140MHz. I'm using a 8MHz crystal oscillator as clock source, below is the source code of the
SystemClock_Config() function from my program. When I bring
RCC_OscInitStruct.PLL.PLLN below ~ 240 my program runs. But when I go up in frequencies my program goes in Hardfault at random places.
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
/**Configure the main internal regulator output voltage */
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 432;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Activate the Over-Drive mode */
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.PLLSAI.PLLSAIN = 192;
PeriphClkInitStruct.PLLSAI.PLLSAIR = 2;
PeriphClkInitStruct.PLLSAI.PLLSAIQ = 2;
PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV4;
PeriphClkInitStruct.PLLSAIDivQ = 1;
PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_2;
PeriphClkInitStruct.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48SOURCE_PLLSAIP;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Configure the Systick interrupt time */
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick */
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 2, 0);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
If you need other part of my program I'd be glad to send it to you, thanks a lot for your help !
Cheers,
Mathieu
Solved! Go to Solution.
2017-04-11 9:14 AM
Check voltage and capacitors on VCAP pins.
Check internal frequency via MCO (PA8) pin.
2017-04-11 7:15 AM
Hi
primitive
,Which CubeMx version are you using ?
Please make sure to use the latest version of CubeMx v4.1 which fixes RCC config issue.
Imen
2017-04-11 9:14 AM
Check voltage and capacitors on VCAP pins.
Check internal frequency via MCO (PA8) pin.
2017-06-23 9:28 AM
Hello Mathieu,
First I thank you for your feedback.
To be able to reproduce it at my end, could you please share your ioc ?
Could you detail a bit your environment (what is your operating system, which cube version are you using, which FMW library) ?
Have you check what CLive has suggested ?
Great thanks in advance.
KR
Sirma
2017-07-13 2:18 AM
Hello Mathieu,
Using STM32CubeMX 4.21 andthe STM32F7 discovery kit for the STM32F746 MCU, I have replicated the configuration of your
SystemClock_Config() function with the exception of the RCC_OscInitStruct.PLL.PLLM setting (because the external clock on the board is 25MHz, therefore I have RCC_OscInitStruct.PLL.PLLM = 25; instead of RCC_OscInitStruct.PLL.PLLM = 8;). With this configuration, my program successfully runs at the system clock frequency of 216MHz (HCLK = 216 MHz max).
When I force the input frequency to 8 MHz and set PLLM to 8 in STM32CubeMX to be in exactly your configuration, the code generated no longer runs on the STM32F7 discovery kit because the external clock is 25 MHz.
Regards,
Angus
P.S. Please find attached my IOC file.
________________ Attachments : F746-DISCO.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyWS&d=%2Fa%2F0X0000000b9b%2Fw5aEg45QkO2hUlzL.WivPHSKpTwzp6ZbBmoYiOvx3tg&asPdf=false2017-10-03 10:26 AM
Thanks a lot, it was indeed a badly soldered VCAP capacitor !