cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4xx ADC Calibration

bnarciso
Associate
Posted on February 21, 2014 at 19:31

I started working with the STM32F4xx and I was wondering if the ADC does a calibration automatically. When I was working with the

STM32F10xx you had to manually trigger the ADC calibration. Looking at the STM32F4xx reference manual there is not a clear answer if the chip does the ADC calibration automatically. The STM32F4xx reference manual also talks about a t STAB, stabilization time after turning on the ADC. Does anybody know that time is? It's not defined in the reference manual.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on February 23, 2014 at 00:20

Hi bn,

This request has to be submitted in the ''STM32'' forum as it is not related to Software topic.

Ragarding the value of STAB, it should be in the datasheet, not reference manaul.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.