2018-06-08 7:32 PM
Hi Everyone,
I am new to stm32f4 series. I have done GPIO example using libraries. But i wanted to do register level programming. I have tried it but i could not get output for this. Can anyone help me out?
&sharpinclude 'main.h'
&sharpinclude 'stm32f4xx.h'&sharpinclude 'stm32f4xx_hal.h' // Device header
void SystemClock_Config(void);
void GPIO_Init(void);int main(void)
{// HAL_Init();
//unsigned int delay=0;SystemClock_Config();
GPIO_Init();while (1)
{ GPIOD->ODR|=0X00004000; //for(delay=0;delay<=16666667;delay++); HAL_Delay(500); //HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_15); GPIOD->ODR&=~0X00004000; // for(delay=0;delay<=16666667;delay++);HAL_Delay(500);}
/* USER CODE END 3 */}
/**
* @brief System Clock Configuration * @retval None */void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}/** Configure pins as
* Analog * Input * Output * EVENT_OUT * EXTI*/void GPIO_Init(void){ RCC->AHB1ENR|=RCC_AHB1ENR_GPIODEN; GPIOD->MODER|=0X1000000;// PIN 14 as output GPIOD->OTYPER|=0X00004000;//Output push pull GPIOD->OSPEEDR|=0X00000000;/ low speed GPIOD->PUPDR&=0X00000000;//no pull up and pull down}
void _Error_Handler(char *file, int line){ /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ while(1) { } /* USER CODE END Error_Handler_Debug */}&sharpifdef USE_FULL_ASSERT
/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, tex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* USER CODE END 6 */}&sharpendif /* USE_FULL_ASSERT *//**
* @} *//**
* @} *//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
#stm32f4discovery #stm32f4 #stm322018-06-13 6:51 PM
Sir, i have tried both the option. But still i could not get the output for ADC.
Please someone help me out to get this output. I have tried my best and still trying.
#include 'stm32f4xx.h'
void GPIO_Init(void);void adc_init(void);
uint16_t adc_read();
uint16_t adc_value1=0,adc_value2=0;int main(void)
{ GPIO_Init(); adc_init();while (1)
{ adc_value2=adc_read(); if(adc_value2>=500) { GPIOD->ODR|=(1<<14); } else { GPIOD->ODR|=(1<<15); } // // GPIOD->ODR&=~(1<<14);// for(delay=0;delay<=4166666;delay++);// GPIOD->ODR|=(1<<15);
// for(delay=0;delay<=4166666;delay++);// // GPIOD->ODR&=~(1<<15);// for(delay=0;delay<=4166666;delay++);}
}
void GPIO_Init(void)
{ RCC->AHB1ENR|=RCC_AHB1ENR_GPIODEN; GPIOD->MODER|=(1<<28); // pin 14 is output GPIOD->OTYPER&=~(1<<14);//pin 14 as push pull GPIOD->OSPEEDR|=(1<<29)|(1<<28);//LOW speed GPIOD->PUPDR&=~(1<<29)|(1<<28);//No push pull GPIOD->MODER|=(1<<30); // pin 14 is output GPIOD->OTYPER&=~(1<<15);//pin 14 as push pull GPIOD->OSPEEDR|=(1<<30)|(1<<31);//LOW speed GPIOD->PUPDR&=~(1<<30)|(1<<31);//No push pullRCC->AHB1ENR |=(1<<0); // clock for gpioA
GPIOA->MODER |= (1<<3)|(1<<2); // Analog mode GPIOA->PUPDR&=~(0X00000000);//No push pull // GPIOA->AFR[0]|=(1<<0)|(1<<1)|(1<<2); // ADC FUNCTION FOR PA1 GPIOA->OTYPER&=~(1<<1);//pin 1 as push pull GPIOA->OSPEEDR|=(1<<3);//HIGH speed }void adc_init(void)
{ RCC->APB2ENR|=(1<<8); ADC1->CR1|=(1<<0)|(1<<23); // 1st CHANNEL // WATCHDOG ENABLE ADC1->CR1&=~(1<<24);// ADC1->CR1|=(1<<24); //10BIT RESOLUTION ADC1->CR2|=(1<<10);// EOCs is set ADC1->SMPR2 |= (1<<3); //15 cycles ADC1->SQR1 &= ~(1<<20); // 1 conversion ADC1->SQR3 = 0x00; }uint16_t adc_read()
{ ADC1->CR2|=(1<<0);// ADC ON ADC1->CR2|=(1<<30);// START CONVERSION while(ADC1->SR&(1<<1)) // wait untill EOC bit set { ADC1->SR = 0X00; adc_value1=ADC1->DR; ADC1->CR2&=~(1<<0);// ADC OFF ADC1->CR2&=~(1<<30);// STOP CONVERSION } return(adc_value1);}2018-06-13 11:26 PM
Maybe you can check here:
https://github.com/turboscrew/blue_pill_init
It's for a 'blue pill' (stm32F103-board), but the other STM32 uC:s should wotk pretty much the same way.But please don't write programs the way I wrote that. The 'program' is rather an executable 'document' to myself.
(Everything in one file, easy to search for text.)
I have never tried the external ADC:s, but the internal temperature sensor (
ADC1_IN16
) works fine.Some other peripherals are used as well.
The DHT-sensor handling is better done by a timer alone and not with GPIOs as it's done there.
The only code that I didn't write myself is 'stdint.h', so no libraries or frameworks.
2018-06-16 4:51 AM
Hi.. Now I am working on STM32F4Doscovery board timers. I want to make a timer interrupt for an application. It can be 1sec or 500ms interrupt. I have read the datasheet and written the program accordingly. But i dont know how to use interrupt in STM32. I have tried something, but nothing is happening. Can someone suggest me a solution??
#include 'stm32f4xx.h'
// Component selectionvoid GPIO_Init(void);
void tim10_init(void);
int main(void)
{GPIO_Init();tim10_init();while (1){GPIOD->ODR|=(1<<15);
}
}
void GPIO_Init(void)
{RCC->AHB1ENR|=RCC_AHB1ENR_GPIODEN;GPIOD->MODER|=(1<<28); // pin 14 is output
GPIOD->OTYPER&=~(1<<14);//pin 14 as push pullGPIOD->OSPEEDR|=(1<<29)|(1<<28);//LOW speedGPIOD->PUPDR&=~(1<<29)|(1<<28);//No push pullGPIOD->MODER|=(1<<30); // pin 15 is output
GPIOD->OTYPER&=~(1<<15);//pin 15 as push pullGPIOD->OSPEEDR|=(1<<30)|(1<<31);//LOW speedGPIOD->PUPDR&=~(1<<30)|(1<<31);//No push pull}void tim10_init(void)
{RCC->APB2ENR|=(1<<17);TIM10->CR1|=(1<<7);TIM10->DIER|=(1<<1);TIM10->SR|=(1<<1);TIM10->EGR|=(1<<1);TIM10->CCMR1|=(1<<3)|(0<<1)|(0<<0);TIM10->CCER|=(1<<0);//TIM10->CCR1=5;TIM10->PSC|=4200;TIM10->ARR|=1000;NVIC_EnableIRQ(TIM1_UP_TIM10_IRQn);}void TIM10_IRQHandler(void){GPIOD->ODR|=(1<<14);}
2018-06-16 7:13 AM