2020-10-14 9:11 AM
Dear all,
I am almost new to SMT32 world.
I would like to use FMC to write to an external DAC, Analog devices AD5447. I attach datasheet for easy reference. It is 12bit, 10Msps and parallel interface.
I am using Nucleo-F439ZI board and STM32CubeIDE to test this. I have configured FMC for NOR Flash/PSRAM/SRAM/ROM/LCD 1, Chip Select: NE1, Memory Type: SRAM, Address: 1 bit, data: 16 bits. I attached the whole project (format .zip) so anyone can have a look.
Just to write data I am using:
/* Write data to the SRAM memory */
HAL_SRAM_Write_16b(&hsram1, DACAddress, aTxBuffer, BUFFER_SIZE);
I tryng to see the waveforms on an oscilloscope but I am not able to see any signal. Can anyone tell me if there is something missing or wrong?
Another question, I would like to write to the DAC on a 5Mhz base, which would the better address/data setup time and bus turn around? I dont see very clear the relation with the datasheet of the AD5447.
Thanks in advance,
Joaquin.
2020-10-19 11:52 PM
Hello All,
I found a problem in my oscilloscope setup, so the I am able to see the signals.
Thanks anyway.
Regards,
Joaquin.
2022-01-21 12:34 PM
I have a similar task here
Your code worked great for me – with one modification:
HAL_SRAM_Write_16b(&hsram1, DACAddress, aTxBuffer, BUFFER_SIZE);HAL_SRAM_Write_16b(&hsram1, SRAM_BANK_ADDR, aTxBuffer, BUFFER_SIZE);Regards,
Franz