cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I-DISC1 Rev. C Changes/Specifications/Documents

evan
Associate II
Posted on January 30, 2018 at 16:13

I just ordered and received REV C of this board, all of the files online seem to indicate they apply to REV B of the board, is anyone aware of the changes or has access to the appropriate files? 

#stm32f429i-disc1
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on January 30, 2018 at 17:44

Practically the same board from the code examples perspective.

The most interesting change (at least for me) is better st-link supporting VCOM (emulated serial port) so you do not need extra hardware to connect to target UART. Also mbed support if you would like to use the board this way.

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee
Posted on January 30, 2018 at 16:32

Hi

Gouzie.Evan

‌,

In

http://www.st.com/content/ccc/resource/technical/document/user_manual/6b/25/05/23/a9/45/4d/6a/DM000939pdf/files/DM000939pdf/jcr:content/translations/en.DM000939pdf

(Discovery kit with STM32F429ZI MCU), you find following details inFigure 9. STM32F429I-DISC1 Discovery board page 28:

0690X00000609Y6QAI.png

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on January 30, 2018 at 17:44

Practically the same board from the code examples perspective.

The most interesting change (at least for me) is better st-link supporting VCOM (emulated serial port) so you do not need extra hardware to connect to target UART. Also mbed support if you would like to use the board this way.