2021-01-03 08:45 PM
I use STM32F429BIT6 controller in our instrument. When Power is ON after initialization STM32F429 controller is Reset. This happen only Once time after power on the instrument. It is not continuous reset.
What can i do
Solved! Go to Solution.
2021-01-05 12:48 AM
You're welcome!
When it works for you and your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Good luck!
/Peter
2021-01-04 01:40 AM
It it not necessary to use an external reset device due to the internal reset circuitry. Please try to remove:
After you've done this, only the reset buttons SW1 and C14 (100nF) are connected to NRST, which is fully sufficient.
/Peter
2021-01-04 09:24 PM
Thank you
2021-01-05 12:48 AM
You're welcome!
When it works for you and your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Good luck!
/Peter