2025-01-20 12:19 PM
Hi I am having the same problem as described in the old post down below.... is there a way to activate the link inside to see the fix?
I am also using the external ULPI PHY, but when the USBD_Connect function executes, pin PB14 is lost. This is becasue the USBD_Connect function is enabling the internal PHY. I know there is a way to fix this but do not remember how. I needed to reinstall the whole environment so the fix was lost and now the code does not work since I need pin PB14 as a GPIO.
Here the post I am referring to:
https://community.st.com/t5/stm32-mcus-products/stm32f4xx-spi2-and-usb-hs-conflict/td-p/438246
Regards
Mark
2025-02-12 2:05 AM - edited 2025-02-12 2:18 AM
Hi @MBurg
It is pointing to this thread
https://community.st.com/t5/stm32-mcus-products/stm32f4-i2s2-pin-af-multiplexer-issue-s/m-p/465934
If OTG_HS_GCCFG_PWRDWN is set (transceiver power down is deactivated) the DM/DP pins are driven by USB.
OTG_HS_GCCFG_PWRDWN is necessary to be set only when using the HS instance.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.