2019-04-19 2:19 AM
Hi everybody,
I'm using STM32F411VE and compiling/debugging with IAR / ST-LINK.
My firmware has a structure that must be non volatile and is, thus, saved on flash everytime the machine detects that the mains have been switched off (by z-crossing detection algorithm).
This structure contains configuration parameters and counters of the machine usage, so these values are real time updated. Everytime I boot my app, the structure is downloaded into a RAM buffer, which is the real interface for my software.
My need is the following: while debugging it's common to reset the microcontroller or to re-flash it again...
1) can i preserve the location in RAM of my buffer in order to retain its state?
2) can i detect, from software, the external reset from the ST-LINK, so I can force a flash write?
Thank you very much
Giuseppe