2025-01-25 02:11 AM - edited 2025-01-25 05:58 AM
Hi Everybody,
I am facing a wired issue in programming the mcu . I have designed a custom borad with STM32F411CEU6 (QFN-48 package). DFU mode is is properly detected. But whenever I am trying to connect the mcu with STM cube programmer in dfu mode mcu gets resets.
Some of the things I have observed:
1. VCAP(1.3067V on vcap pin) Voltage drops by 0.3V while trying to connect with cube programmer.
2. MCU connects easily if I apply a little bit of heat . Disconnects again as soon as the mcu cools down. This kind of behaviour I have never seen with ST mcu.
3. DFU mode successfully deteted by the pc.
Actions taken :
1. MCU supply voltage check: The supply voltage is steady . No fluctuation observed.
2. HSE crystal and their values checked with different capacitors values.
3. Able to donload the firmware using STLINKV2.
4. But MCU remains under reset.
3. I have 3 samples of the mcu . Result is same with all of them.
I have attached the schematic and pcb layout along with this post. The hardware is tested already with previous pcb design. Due to some size issue I had to change the layout and found this issue.This is the new layout with fresh components.This is my second iteration. I will be very greatfull if you could guide me a little bit.
2025-01-25 04:44 AM
VBAT require be connected to 3V3 too.
2025-01-25 05:07 AM - edited 2025-01-25 05:08 AM
Hello MM..1, Thanks for your repsonse.
We have already tested the hardware in our previous pcb design. Now only the layout hase been changed. Not the circuit. The issue is comming in new layout. But i will try out your suggestion.
2025-01-25 09:20 AM
Sounds like a hardware assembly issue. VCAP dropping suggests insufficient or invalid power. Perhaps a VSS connection is flaky. NRST pulsing suggests the chip is resetting internally likely due to a power issue.
Does SWD mode work?
Does 3V3 also drop when trying to connect? (Use a scope to see if drops correspond to NRST.)
2025-01-25 10:06 AM - edited 2025-01-25 10:09 AM
SWD works fine. I am able to download the firmware. But mcu remains in reset mode . MCU doesn't excute the program. 3.3V supply doesn't drop during connection. DFU mode is detected by the PC .But MCU resets when I try to connect with cube programmer. I have attached VCAP voltage waveform , and 3.3V line wave form for refferance. 3.3V line stays stable during entire operation. MCU connects with cube programmer in dfu mode if I apply a little bit of heat over the mcu and able to download the firmware. MCU remains connected as long as it is warm . Connection disconnectes as soon as mcu cools down. May be mcu's internal voltage regulator not working properly due to some reason.
3.3V waveform (Completely stable...no disturbances observed)
.
VCAP waveform
2025-01-25 03:03 PM
> MCU connects easily if I apply a little bit of heat . Disconnects again as soon as the mcu cools down. This kind of behaviour I have never seen with ST mcu.
Very unusual indeed. Hints to a shorting somewhere. When you apply heat, things expand and the shorting disappears. Something like that
2025-01-26 06:13 AM - edited 2025-01-26 06:13 AM
May be.But where the short is, can't figure out. Can't find any trace of short with measurement. Everything looks ok. The board connects with PC . Windows shows "ST BOOTLOADER " in deice manager list . Where the issue is comming from dont' know. Anyway I am still trying to figure out . Thanks for your reply.
2025-01-26 08:23 AM
This isnt short,but cold junction = not connected in cold state. Try resolder MCU with some soldering liquid , after solder use clean liquid (alcohol based)
2025-01-26 08:52 AM - edited 2025-01-26 08:53 AM
Okay. I will do that. Thanks for pointing out that.Will let you know the result.
2025-01-28 09:28 AM
The issue has been solved . VCAP capacitor gorund was missing on pcb. I have soldered a piece of wire to connect vacp negative to ground. Thank you every one for your valuable suggestions .