2024-06-04 11:33 PM - last edited on 2024-06-05 12:09 AM by Peter BENSCH
@
STM32Cube_FW_F4_V1.28.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw
I use this Demo,replace phy with Lan8742 sucessfully,then I ping this board ip address sucessfully too,but when I open webpage by browser,the network is down,cannot ping ,how to solve this problem。
with
STM32Cube_FW_F4_V1.26.2\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw
this version can work whole time.Compare two versions,different files are HAL Drivers and ethernetif.c.so
how to solve this problem,thanks for your help!
Solved! Go to Solution.
2024-07-04 5:57 AM
Hello @ZainFan ,
by costume board I mean is this a Custom PCB that you are using this is not a board provided by ST so you need to make sure that you are rooting the correct pins to the PHY interface are the same (check pinouts in the Ethernetif.c to look for changes as the example you put don't use the same PHY. also make sure you are using the correct lan8720.c file.
Regards
2024-06-13 8:12 AM
Hello @ZainFan ,
thank you for sharing this with us.
could you please give us some details to help us reproduce you issue?
about the Hardware you are using?
is the STM32F407ZGT6 +LAN8720 a custom board?
Regards
2024-06-17 2:05 AM
sorry ,idont know what is a custom board? I buy it online。i can support a link to my code。
https://github.com/zainFan/STM32.git
thanks for your help ,you can find me with my email 1019472847@qq.com
2024-06-18 5:37 PM
yes,my hardware is STM32F407ZGT6 +LAN8720
2024-07-04 5:57 AM
Hello @ZainFan ,
by costume board I mean is this a Custom PCB that you are using this is not a board provided by ST so you need to make sure that you are rooting the correct pins to the PHY interface are the same (check pinouts in the Ethernetif.c to look for changes as the example you put don't use the same PHY. also make sure you are using the correct lan8720.c file.
Regards
2024-08-02 4:19 AM
Hello @ZainFan,
Did you manage to solve this issue? is there any updates?
Regards