2017-03-30 10:13 PM
Hi everyone,
I wanted to move a data array(source) to another data array(destination) using USART2 and I wanted to move datas to usart2 and from usart2 by using DMA1. I connect the tx pin to rx pin and it worked. The thing confused me is when I disconnected pins somehow some of the datas were able to go to destination array.
My code is below. Can you explain me what is going on?
&sharpinclude <stm32f4xx.h>
int sayac = 0;int main(){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; DMA_InitTypeDef DMA_InitStructure; uint8_t source[500] = 'Hello WorldHello World Hello World Hello World Hello World Hello WorldHello WorldHello WorldHello World Hello World Hello World Hello WorldHello WorldHello WorldHello WorldHello World Hello World Hello World Hello World Hello World Hello World etc..
'; uint8_t destination[500] = {0}; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,ENABLE); //GPIO Initialisation for USART GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_Init(GPIOD,&GPIO_InitStructure); GPIO_PinAFConfig(GPIOD,GPIO_PinSource5,GPIO_AF_USART2); GPIO_PinAFConfig(GPIOD,GPIO_PinSource6,GPIO_AF_USART2); //USART Initialisation USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_Init(USART2,&USART_InitStructure); USART_Cmd(USART2,ENABLE); //DMA Stream6 Initialisation for USART Tx DMA_DeInit(DMA1_Stream6); while(DMA_GetCmdStatus(DMA1_Stream6) != DISABLE); DMA_InitStructure.DMA_Channel = DMA_Channel_4; //channel of the stream DMA_InitStructure.DMA_Priority = DMA_Priority_High; //select priority of the stream DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)source; //address of source DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR; //address of peripheral DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral; //Direction of the transfer DMA_InitStructure.DMA_BufferSize = sizeof(source); //amount of data to be sent DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; //Enable incremantation of memory address DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; //Disable incremantation of peripheral address DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; //verinin boyutu DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; //verinin boyutu DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; //Stream is disabled when Transfer finishes DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; //Fifo disable oldugu i�in �ok �nemli degil DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; //minumum burst miktar1 yaz1lmazsa olmuyor DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; //minumum burst miktar1 yaz1lmazsa olmuyor DMA_Init(DMA1_Stream6,&DMA_InitStructure); //DMA Stream5 Initialisation for USART Rx DMA_DeInit(DMA1_Stream5); while(DMA_GetCmdStatus(DMA1_Stream5) != DISABLE); DMA_InitStructure.DMA_Channel = DMA_Channel_4; //channel of the stream DMA_InitStructure.DMA_Priority = DMA_Priority_High; //select priority of the stream DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)destination; //address of source DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR; //address of peripheral DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; //Direction of the transfer DMA_InitStructure.DMA_BufferSize = sizeof(destination); //amount of data to be sent DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; //Enable incremantation of memory address DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; //Disable incremantation of peripheral address DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; //verinin boyutu DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; //verinin boyutu DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; //Stream is disabled when Transfer finishes DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; //Fifo disable oldugu i�in �ok �nemli degil DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; //minumum burst miktar1 yaz1lmazsa olmuyor DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; //minumum burst miktar1 yaz1lmazsa olmuyor DMA_Init(DMA1_Stream5,&DMA_InitStructure);USART_ClearFlag(USART2,USART_FLAG_RXNE);
USART_ClearFlag(USART2,USART_FLAG_TXE); USART_DMACmd(USART2,USART_DMAReq_Rx,ENABLE); USART_DMACmd(USART2,USART_DMAReq_Tx,ENABLE);DMA_Cmd(DMA1_Stream6,ENABLE);
DMA_Cmd(DMA1_Stream5,ENABLE); while(1) { }}#stm32f407vg-using-usart-with-dma*2017-03-30 11:30 PM
>>Can you explain me what is going on?
Not really. Make sure your stack is large enough to contain the arrays, or use statics.
2017-03-30 11:40 PM
hi K.M....
You receivi the data from DMA method ,after the receiving data clear DMA DR regester
2017-03-31 12:37 AM
I suspect it si something with USART_DR. USART have one register for Transmit and recieve. Dma is writing datas from memory to this register to transmit and reading recieved datas from this register to another memory place. I don't understand how does usart handle full duplex transfer like my example with only one register.
2017-03-31 12:55 AM
To make it clear.
Usart2 Tx connected to USART2 Rx(array size 500)
Usart2 Tx is not connected to USART2 Rx(array size 500)
Usart2 Tx is not connected to USART2 Rx
(array size 250)
2017-03-31 01:19 AM
Try to switch on the pullup on the Rx pin.
JW
2017-03-31 01:29 AM
Wow. It worked. What is the difference?
2017-03-31 01:36 AM
Thank you very much. I woukdn't guess that. I was thinkin there is one register for both transmit and recieve thats why DMA is somehow taking the data it's just wrote.
Thank you again.
2017-03-31 03:01 AM
Method 1 : usart normal method it works on only one register USART_DR register...
Method 2 :your using in DMA it works on DMA USART Tx and Rx DR Registers
2017-03-31 03:31 AM
You were 'receiving' through some parasitic (capacitive?) coupling between Tx and Rx.
JW