2017-04-05 7:23 AM
Hello all,
I'm using STM32F407VGT6, with 32-bit ARM� Cortex�-M4 microcontroller.
I would need support with implementation of UART for this microcontroller.
I couldn't find clear step tutorial for this task.
To focus on, on this MCU I am using UART4 module I would need only Initialization and UART4 write text methods.
Feel free to ask for more information.
P.S. I hope I didn't make duplicate thread, if so I feel sorry.
Thanks in advance!
#uart #stm32f4 #uart.stm32-uart2017-04-06 5:37 AM
Hi
lukadragicevic032@mail.com
,STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Examples\UART
UART
Initialization using
which is a graphical software configuration tool that allows generating C initialization code using graphical wizards.-Nesrine-
2017-04-06 6:02 AM
All the U(S)ART are reasonably consistent, apply common methods and tailor to specific pin and peripherals