cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 TIM / PWM Problem

CKILI.2
Associate II

Hi everyone,

For any timer, counter mode is equal to center aligned mode 3/2/1 except for up or down there are phase sub. between pwm channels with different duty values. There is no phase sub channels with same duty values.

 

For example, in TIM1 with center aligned mode 3, I have selected channel 1 and channel 2 for pwm generation, Arr =100, there is phase sub for

TIM1->CCR1=50 and TIM->1CCR2=75, 

there are no phase sub same values and up/down counter mode.

 

Thank's for valuable comments.

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @CKILI.2

I'm not sure I've understood the issue here.. 

Since both channels have the same compare value (CCR1 = CCR2 ), the PWM signals for both channels will toggle at the same points in the counting period. Therefore, there will be no phase shift between the two signals.

The absence of phase shift is due to the synchronized toggling of the two PWM signals, which occurs because the compare match events are aligned. 

Does that answer your question? otherwise, could you explain more!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Sarra.S
ST Employee

Hello @CKILI.2

I'm not sure I've understood the issue here.. 

Since both channels have the same compare value (CCR1 = CCR2 ), the PWM signals for both channels will toggle at the same points in the counting period. Therefore, there will be no phase shift between the two signals.

The absence of phase shift is due to the synchronized toggling of the two PWM signals, which occurs because the compare match events are aligned. 

Does that answer your question? otherwise, could you explain more!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.