Skip to main content
vchau.2
Associate III
Aug 27, 2024 5:07 PM UTC
Solved

Over flow flash memory

Dear All,

I'm using STM32G0 with 64KB of flash memory and 8KB of RAM

if optimization is OFF, its giving error as below

vchau2_0-1724778215817.png

 

and if optimization is ON Level-1 

its not giving any error

vchau2_1-1724778336673.png

So let me know what kind of error i'm facing 

Compiler - keil

 

This topic has been closed for replies.
TDK
TDKBest answer
Aug 27, 2024 5:37 PM UTC

> Over flow flash memory

> So let me know what kind of error i'm facing 

You answered it yourself. The code is larger than the flash size you have available.

Potential solutions:

  • Refactor the code to use less memory
  • Compile with optimizations on
  • Buy a chip with more flash
"If you feel a post has answered your question, please click ""Accept as Solution""."

5 replies

mƎALLEm
ST Technical Moderator
Aug 27, 2024 5:35 PM UTC

Hello,

Simply you are exceeding the flash memory size.

In fact your application is at the limit of the flash size 64kB. If you enable the optimization your binary < 64kB and that fits in the Flash and if you disable the optimization, the binary > 64kB exceeding the memory size of the MCU.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
vchau.2
vchau.2Author
Associate III
Aug 28, 2024 3:58 AM UTC

But when optimization is of level-1 than occupy flash size is 27KB only, how its possible to optimize the code size more than half 

mƎALLEm
ST Technical Moderator
Aug 28, 2024 6:35 AM UTC

Hello,

Maybe you need to contact ARM for such kind of behaviour over this link:

https://community.arm.com/support-forums/f/keil-forum

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
TDKBest answer
Aug 27, 2024 5:37 PM UTC

> Over flow flash memory

> So let me know what kind of error i'm facing 

You answered it yourself. The code is larger than the flash size you have available.

Potential solutions:

  • Refactor the code to use less memory
  • Compile with optimizations on
  • Buy a chip with more flash
"If you feel a post has answered your question, please click ""Accept as Solution""."
gbm
Super User
Aug 28, 2024 7:17 AM UTC

My guess is: you are using trial/resrticted version of MDK-ARM with 32 KiB size limit.

Solutions:

1. Switch to STM32CubeIDE.

or

2. Enable STM32F0/G0 license. This will unlock the size limit but lock your MDK-ARM to F0/G0, so you won't be able to use it with any other microcontroller.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice