2015-03-18 4:33 AM
Hi
I'm using a STM32F405RG in a fan controller, I've two fans tacho outputs connected via opto-isolators to Pins, I wish to count the number of falling edges per second.PA5 (Tim2 CH1 ext clock source mode 1, trigger on TI1FP1) all other Tim2 pins disabledPB6 (Tim4 CH1 ext clock source mode 1, trigger on TI1FP1) all other Tim4 pins disabledboth have interrupts enabled for Trigger event TIMx_DIER = 0x0040on a falling edge as this is cleaner than rising edge, TIMx_SMCR = 0x8057Timers are running in interrupt mode (HAL_TIM_Start_IT(&htimX))A third timer reads the htimX.Instance->CNT once a second and returns a value in Hz.The problem is that this value is unreliable, a 10Hz square wave input mimics an expected input. 5Hz reads as 293.1Hz reads as 1.10Hz reads as 4698.My understanding is that in ext Time mode 1, an interrupt is generated for each edge detected, I've tried using the filter setting to reduce the likelihood of multiple triggers per edgebut to no avail. Using a timer to disable the interrupt for 200uS after an edge also proved unfruitful.Page 590 of the reference doc RM0090 describes the feature I'm trying to use.Any help would be appreciated. #stm32f405rg-pulse-counter-timx #stm32f4052015-03-19 7:03 AM
void
edgeCountSetup(TIM_HandleTypeDef *htim){
//setup timers for edge counting on falling edge
htim->Instance->CR1 &= ~0xFFF9;
//disable timer while writing changes
htim->Instance->CR2 &= 0xFF20;
// TI1 input, update event = TRGO
htim->Instance->CR2 |= 0x0020;
htim->Instance->DIER &=0x0040;
// disable other interupts
htim->Instance->DIER |=0x0040;
// set ext trigger interrupt
htim->Instance->SMCR &= 0x8050;
htim->Instance->SMCR |= 0x8057;
// falling adge, Filter Timer In 1, ext Clk Mode 1
htim->Instance->SR &= 0x0000;
// clear flags
htim->Instance->EGR &= 0x0000;
// clear events
htim->Instance->CCER &= 0x0000;
// disable capture compare
htim->Instance->CNT &=0x0000;
// reset count
htim->Instance->PSC &=0x0000;
// prescale 1:1
htim->Instance->ARR |=0xFFFFFFF0;
// counter is blocked if this is 0
htim->Instance->OR &= 0x0000;
// option reg cleared
htim->Instance->CR1 |= 0x0001;
//enable timer
}
This is used to configure timer 2 and timer 5,
As said previously, the htim.Instance->CNT does respond to an incoming signal but not in a single increment per falling edge. The fall/rise time of my signal is about 20uS, Setting up 2 other timers in one shot mode to disable the trigger interrupt for 50uS has not cleaned up the results.