2016-04-25 8:25 AM
Hi,
We are experienced STM32 developers but we are having a real problem connecting to a new card, containing an STM32F405OE device. (the WLCSP 90 pin package). No matter what we have tried, the ST-LINK utility (v3.8.0) will not compete it;s connection to the device (using the SW interface). Looking at the debug trace (attached) we see that it appears to succeed in communicating with the chip, but then reaches the reset stage and fails. We have scoped the VCAP pins and they are at 1.2V. The NRST pin rises very nicely to 3.3V and we can see SWCLK and SWIO switching using a scope. Has anyone seen a similar issue or can anyone advise as to what the trace means. Thanks #stm32f405oe-debug-serial-wire2016-04-25 9:31 AM
Has anyone seen a similar issue or can anyone advise as to what the trace means.
We seem to get people here, at least briefly, that suffer from all sorts of problems. I know I've gone over it dozen and dozen of times over the years.The attachment doesn't seem to be working right now, the site is in transition. Try using pastebin.Have you done any other basic signs of life tests, like use the ROM by pulling BOOT0 High and seeing if you can talk to the loader via USART1 or USART3, or connecting the USB-FS in DFU mode?2016-04-25 9:33 AM
Could you please resend the attachment (the debug trace).
Best Regards,Tarek2016-04-26 12:56 AM
2016-04-26 1:35 AM
Apologies for above link
this was a trace that didn't have any repliesthe trace that shows a conversation is http://pastebin.com/rzYaKcVTThanks