cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405 ETH pkt receive but not transmit

khorght
Associate II
Posted on August 08, 2013 at 19:27

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
1 REPLY 1
Posted on December 16, 2014 at 11:18

Hi Sergey.

I have the same type of problems:

- in 10Base-T the board work fine

- in 100Base-TX mode the RX is OK but the PHY never transmit over the network ...

Have you a solution for this type of problem ?

Thanks.

Paolo