cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401RCT6 use at 2.8v

Kris1
Associate II
Posted on July 15, 2016 at 12:43

Hi ,

      I want to use STM32F401RCT6 at 2.8 V, which is compatible with VS1053 Audio Codec IC, Please Suggest Can I use it with 2.8V.

#stm32f401-audio-codec
2 REPLIES 2
Amel NASRI
ST Employee
Posted on July 15, 2016 at 14:51

Yes it should be possible.

refer to the table ''General operating conditions'' in

http://www.st.com/content/ccc/resource/technical/document/datasheet/9e/50/b1/5a/5f/ae/4d/c1/DM00086815.pdf/files/DM00086815.pdf/jcr:content/translations/en.DM00086815.pdf

for more details.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Kris1
Associate II
Posted on August 01, 2016 at 08:01

Hi mayla,

     Thank you for Reply.