cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4: Using several ADCs independent

alexanderjonas
Associate II
Posted on May 28, 2016 at 12:59

Hello,

I wonder if it is or it is not possible to use more than one ADC independet of each other.

My problem is as follows:

I want to use ADC1 and ADC2 in dual mode and ADC3 in independent scan conversion mode. I can successfully ADC1 and ADC2 in dual mode but as soon as I also initialize ADC3 in independent mode, nothing works anymore. My code for ADC3 alone, without using ADC1 and ADC2, also works well. It has to be added, that I use DMA for all ADCs.

I don't see whre the problem is...

#independend #adc #stm32f4
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 28, 2016 at 14:37

Common initialization must only be done once. Dual mode infers third unit is independent.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..