2013-11-14 7:56 PM
Hello,
I have been busy these past days trying to understand a problem revolving around this simple algorithm : every second write a byte through SDIO using ST DMA2 example. Using a simple loop in main works perfectly : while(1) file.write(1); But using a TIM interrupt fails : void TIM7_IRQHandler(void) { file.write(1); } The operation hangs in : SD_WaitReadOperation(void) first while loop checking for the DMA transfer end : while ((DMAEndOfTransfer == 0x00) && (TransferEnd == 0) && (TransferError == SD_OK) && (timeout > 0)) It seems the DMA2 interrupts aren't triggered when the context is the TIM interrupt. The preemption priorities are : - SDIO_IRQn : 0 (ST example), - SDIO SD_SDIO_DMA_IRQn: 1 (ST example), - TIM_IRQn : 11. The MCU is STM32F407VET6 and DMA is only used for SDIO. The same problem happens when the context is an USART interrupt. Is this expected behaviour ? Thank you very much ! #stm32 #sdio #interrupt #dma