cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 DMA and Varying Duty Cycle

haseebnain
Associate II
Posted on June 28, 2016 at 03:09

Hi everyone,

I am wondering how to go about setting up a varying duty cycle on an F4 board using the DMA. This is for a personal project of mine, I have asked around and believe my code does not have any glaring logic issues but it still does not vary the duty cycle of the timer. For the purpose of this project I need to use TIM5 (projecting the output PWM to PA0). I attempted using Channel 6 and Stream 0 but cannot as something is already using PA2 not allowing me to mess with TIM5_CH3.

//initialize structs
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
uint16_t prescalerValue;
//enable GPIOA clock
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
//enable TIM5 clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM5, ENABLE);
//enable DMA1 clock
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);
/* GPIOA Configuration: TIM5 Channel 1 as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM5);
// Stop timer
TIM_Cmd(TIM5, DISABLE);
/* Compute the prescaler value */
prescalerValue = (uint16_t) (SystemCoreClock / 2 / 84000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 104; 
// 800kHz
TIM_TimeBaseStructure.TIM_Prescaler = prescalerValue;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM5, &TIM_TimeBaseStructure);
/* PWM1 Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 0;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM5, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM5, TIM_OCPreload_Enable);
//TIM5->CCR2 = 106;
TIM_Cmd(TIM5, ENABLE);
/* configure DMA */
/* DMA1 Channel Config */
/* DMA1 Stream6 setup*/
DMA_Cmd(DMA1_Stream6, DISABLE); 
// disable DMA channel 6
DMA_DeInit(DMA1_Stream6);
DMA_StructInit(&DMA_InitStructure);
DMA_InitStructure.DMA_Channel = DMA_Channel_6;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(TIM5->CCR1);
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ledStripDMABuffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral;
DMA_InitStructure.DMA_BufferSize = WS2811_DMA_BUFFER_SIZE;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_1QuarterFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA1_Stream6, &DMA_InitStructure);
DMA_ITConfig(DMA1_Stream6, DMA_IT_TC, ENABLE);
DMA_ClearITPendingBit(DMA1_Stream6, DMA_IT_TCIF6); 
// clear DMA1 Channel 6 transfer complete flag
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream6_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = NVIC_PRIORITY_BASE(NVIC_PRIO_WS2811_DMA);
NVIC_InitStructure.NVIC_IRQChannelSubPriority = NVIC_PRIORITY_SUB(NVIC_PRIO_WS2811_DMA);
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);

My desire is to update the duty cycle every time the timer update occurs, the value of that duty cycle should be updated with the value of the

ledStripDMABuffer

. Is there something obvious I am missing? #stm32f4-dma-timer
10 REPLIES 10
Posted on July 01, 2016 at 22:57

It is certainly possible to chase the phase angle of the timer, I'd use TIM1_UP as the trigger to load the duty once per cycle.

Not an F3 user, as the frequency increases the contention on the bus is going to have a deleterious effect on system performance.

I think I've demonstrated 21 MHz PWM on the F4, pretty sure I wasn't modulating on a per cycle basis though. One could decimate the loading using a repetition count.

People have modulated bit streams with SPI and pattern buffers.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..