Stm32F4 DMA+ADC cannot work
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-05-09 3:25 AM
Posted on May 09, 2014 at 12:25
Hi all.
I'm trying to work with ADC and DMA. The adc works, i'm able to read directly value form pin PC1. When i try to read it using DMA a get alway zero value. I'm try to get work example from stm32f4_dsp_stdperiph_lib but nothing. I'm newbe. Someone could give me an hint. The source i use is this: tatic void ADC_Config(void) { ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable ADCx, DMA and GPIO clocks ****************************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); /* DMA2 Stream0 channel2 configuration **************************************/ DMA_InitStructure.DMA_Channel = DMA_Channel_2; DMA_InitStructure.DMA_PeripheralBaseAddr = ((uint32_t)0x4001204C); DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&uhADCxConvertedValue; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream0, &DMA_InitStructure); DMA_Cmd(DMA2_Stream0, ENABLE); /* Configure ADC3 Channel7 pin as analog input ******************************/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* ADC Common Init **********************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC3 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); /* ADC3 regular channel7 configuration **************************************/ ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 1, ADC_SampleTime_3Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE); /* Enable ADC3 DMA */ ADC_DMACmd(ADC1, ENABLE); /* Enable ADC3 */ ADC_Cmd(ADC1, ENABLE); } int main(void) { #if defined(DEBUG) /* * Send a greeting to the standard output (the semihosting debug channel * on Debug, ignored on Release). */ printf(''Hello ARM World!\n''); #endif /* ADC configuration */ ADC_Config(); /* Start ADC Software Conversion */ ADC_SoftwareStartConv(ADC1); /* * At this stage the microcontroller clock setting is already configured, * this is done through SystemInit() function which is called from startup * files (startup_cm.c) before to branch to the * application main. To reconfigure the default setting of SystemInit() * function, refer to system_stm32f4xx.c file. */ RCC_ClocksTypeDef RCC_Clocks; /* Use SysTick as reference for the timer */ RCC_GetClocksFreq(&RCC_Clocks); SysTick_Config(RCC_Clocks.HCLK_Frequency / SYSTICK_FREQUENCY_HZ); /* GPIO Periph clock enable */ RCC_AHB1PeriphClockCmd(BLINK_RCC_BIT, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; /* Configure pin in output push/pull mode */ GPIO_InitStructure.GPIO_Pin = (1 << BLINK_PIN); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(BLINK_PORT, &GPIO_InitStructure); int seconds = 0; /* Infinite loop */ while (1) { uwADCxConvertedVoltage = uhADCxConvertedValue *3300/0xFFF; #if defined(DEBUG) /* * Count seconds on the debug channel. */ printf(''ADC value = %d\n'', uwADCxConvertedVoltage); #endif if (uwADCxConvertedVoltage >0) { /* Turn on led by setting the pin low */ GPIO_ResetBits(BLINK_PORT, (1 << BLINK_PIN)); Delay(BLINK_TICKS); /* Turn off led by setting the pin high */ GPIO_SetBits(BLINK_PORT, (1 << BLINK_PIN)); Delay(BLINK_TICKS); } ++seconds; #if defined(DEBUG) /* * Count seconds on the debug channel. */ printf(''Second %d\n'', seconds); #endif } } Thanks in advance. Carmelo.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-05-09 4:21 AM
Posted on May 09, 2014 at 13:21
Hi all.
I think i foud my error: Wrong DMA channel: DMA_InitStructure.DMA_Channel = DMA_Channel_0; Thanks Carmelo