2018-11-10 4:02 AM
This failure happened suddenly with no apparent cause. The board started cycling on/off at a fairly regular frequency (as shown in the attached video). When this happened, LD1, LD2, and LD7 all cycled on/off (LD7 never turns on in normal operation, and I don't use CN5).
I changed the cable, and the problem appears solved. However, I use an FTDI board to communicate. When I used the cable I used with the Discovery board with it instead, at first it worked with no problem. After a while, however, the same problem appeared, with the Discovery board turning on and off (with no apparent change in the FTDI board, which was connected to this cable). Then I used a different cable with it, and the problem appears to be gone for now.
My questions are,
Thank you very much for reading this, and I appreciate any help I can get.
2018-11-10 5:18 AM
change the power supply...
2018-11-10 5:19 AM
The power supply is via the USB cable connected to the laptop.
2018-11-10 5:26 AM
So perhaps continuity issues with the cable/connector. Issues with excessive loading on the regulator. Issues with the soldering and/or components on the board.
Issues with the supply on the laptop.
Try running the board from a USB charger (use current fw)
2018-11-10 5:39 AM
If the board has a problem, you could use your finger to check if something is hot.
otherwise, a nice big power supply should be able to pinpoint the issue for you...
just make sure you have safety glasses on first.