cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F37x: What is ''tempo'' or probably temporization for the clocks

Uwe Bonnes
Principal III
Posted on January 07, 2013 at 18:17

Hello,

rm0313 in figure 10 ''Clock tree part1'' has a ''tempo'' unit at each clock input. Beside a use of  the word ''temporization'' in 7.2.11 ''Watchdog clock'', I see no more use of that word and no explication at all.

What is this ''temporization''?

Thanks

#unclear-term #poor-documentation
4 REPLIES 4
Posted on January 07, 2013 at 19:50

What is this ''temporization''?

''

the act of delaying

''

In the context used classically by ST it means a delay for the purposes of stabilization, in the case of the clocks the F1's LSI needs an additional 100us to become truly stable.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 07, 2013 at 22:48

That doesn't seem to make much sense in the context of the figure to which

0690X0000060MlxQAE.gifwas referring?

John F.
Senior
Posted on January 08, 2013 at 09:31

Makes sense to me. Both the LSI and LSE oscillators will take a finite time to start and become stable after they have been enabled. For example, the LSIRDY flag in the Control/status register (RCC_CSR) indicates if the LSI oscillator is stable or not. At startup, the clock is not released until this bit is set by hardware.

Presumably the ''tempo'' blocks handle this functionality.

Posted on January 08, 2013 at 11:31

OK - now I see.

But it remains very poor that we should have to guess at this stuff - it should be clearly & explicitly stated in the documentation.