cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F334 RTC Prescaler, Bug in Datasheet ?

Manu Abraham
Senior
Posted on April 17, 2017 at 19:36

Hi,

While trying to calibrate the RTC on the F334, tripped on this rather possible bug..

I guess this is a bug in the Application Note AN3371

Doc ID 018624 Rev 5

Figure 11. Smooth calibration block, the RTCCLK is assumed to be 32768,

as well as in

Figure 18. RTC_CALIB clock sources

Just above Fig 18, it also states:

Setting 1 Hz as the output signal

1. Select LSE “32768 Hz� as the RTC clock source.

2. Set the asynchronous prescaler to the default value “128“.

3. Set the synchronous prescaler to the default value “256“.

4. Enable the output calibration by setting “COE� to ‘1’.

5. Select 1 Hz as the calibration output by setting CALSEL to ‘1’.

But, according to the datasheet RM0364, DocID025177 Rev 2

RTC prescaler register (RTC_PRER)

Bits 22:16 PREDIV_A[6:0]: Asynchronous prescaler factor

This is the asynchronous division factor:

ck_apre frequency = RTCCLK frequency/(PREDIV_A+1)

Bit 15 Reserved, must be kept at reset value.

Bits 14:0 PREDIV_S[14:0]: Synchronous prescaler factor

This is the synchronous division factor:

ck_spre frequency = ck_apre frequency/(PREDIV_S+1)

Asynchronous prescaler is 7 bits wide. Setting '128' will overflow the bitfield, but setting 127 (0x7f) does seem correct.

But, 32768/128 = 256Hz, but the figure states 512Hz.

Isn't this a bug in the document ? Is there an already update to the Application Note already available ?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on April 20, 2017 at 09:33

Table 3 uses '127 (div128)', and 'divXXX' is used on many places of the AN.

Not a bad idea, but shall be explained in the AN's introduction, and then be used consistently - there are many places where the divider is used without the 'div' prefix (including the figures).

ST, please comment.

JW

Imen.D
ST Employee
Posted on April 21, 2017 at 18:33

Hi

Abraham.Manu

,

Waclawek.Jan

,

I want to thank you for your contribution. This is helpful for us to improve our doc offers.

I will raise your feedback internally.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen