STM32F302R8 - Not giving DAC output.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-21 8:50 PM
I am using the STM32F302R8 for motor control application. Need to do pulse-by-pulse current limiting.
I have a BLDC drive board that has a comparator that can be used to give shutdown signal to the PWM. For this purpose, I need to give the comparator a reference signal from DAC of microcontroller.
Using STMCubeIDE to configure the peripherals.
DAC Mode - OUT1 Configuration
Parameter Settings - Output Buffer Enabled
Trigger - Software Trigger
Wave Generation - Disabled
Then, I use
HAL_DAC_Start(&hdac, DAC_CHANNEL_1);
HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4096);
in the main() to start and set the values of the DAC. But the output is showing 0V instead of 3.3V.
I have set the DAC value to 4096 to check output only. I know that I can use the internal reference voltage from microcontroller for Vref, 3/4 Vref, 1/2 Vref etc..
I need a very specific voltage reference for the comparator, I cannot use standard values.
If any has found a solution to the DAC output problem, I'd be grateful for the help.
Thanks =)
- Labels:
-
DAC
-
STM32F3 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-22 7:58 AM
Hello
fill first the data register and then , start the conversion
HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4096);
HAL_DAC_Start(&hdac, DAC_CHANNEL_1);