2018-09-30 4:33 AM
Hello
I am trying to trigger adc with injected mode using TIM1 CCR 4 event.When i try to use TIM1 upgrade to generate injected ADC interrupt it worked.I used event 0 for adc injected.But when i try to use TIM1 CCR 4 event to trigger injected ADC it is not working.Here is my code.
void TIM1_Init(void)
{
TIM_OCInitTypeDef TIM_OCInitStruct;
TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct;
NVIC_InitTypeDef NVICStruct;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1,ENABLE);
TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInitStruct.TIM_Period = 63;
TIM_TimeBaseInitStruct.TIM_Prescaler = 99;
TIM_TimeBaseInitStruct.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM1,&TIM_TimeBaseInitStruct);
TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStruct.TIM_OCIdleState = TIM_OCIdleState_Reset;
TIM_OCInitStruct.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStruct.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
TIM_OCInitStruct.TIM_OCNPolarity = TIM_OCNPolarity_High;
TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStruct.TIM_OutputNState = TIM_OutputNState_Enable;
TIM_OCInitStruct.TIM_Pulse = 20;
TIM_OC4Init(TIM1,&TIM_OCInitStruct);
TIM_OC4PreloadConfig(TIM1,TIM_OCPreload_Enable);
NVICStruct.NVIC_IRQChannel = TIM1_UP_TIM16_IRQn;
NVICStruct.NVIC_IRQChannelPreemptionPriority = 1;
NVICStruct.NVIC_IRQChannelSubPriority = 0;
NVICStruct.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVICStruct);
TIM_SelectMasterSlaveMode(TIM1,TIM_MasterSlaveMode_Enable);
//if i try to use TIM_TRGOSource_Update as trigger it works.
TIM_SelectOutputTrigger(TIM1,TIM_TRGOSource_OC4Ref);
TIM_ITConfig(TIM1,TIM_IT_Update,ENABLE);
TIM_CtrlPWMOutputs(TIM1,ENABLE);
TIM_Cmd(TIM1,ENABLE);
}
void ADC_Injected_Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStruct;
NVIC_InitTypeDef NVIC_InitStruct;
ADC_InjectedInitTypeDef ADC_InjectedInitStruct;
/* Enable ADC1 clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
ADC_CommonInitStruct.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStruct.ADC_TwoSamplingDelay =0x0;
ADC_CommonInitStruct.ADC_DMAAccessMode =ADC_DMAAccessMode_Disabled;
ADC_CommonInitStruct.ADC_Clock = ADC_Clock_AsynClkMode;
ADC_CommonInit(ADC1,&ADC_CommonInitStruct);
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfRegChannel = 1;
ADC_Init(ADC1, &ADC_InitStructure);
NVIC_InitStruct.NVIC_IRQChannel = ADC1_2_IRQn;
NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;
NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStruct.NVIC_IRQChannelSubPriority = 2;
NVIC_Init(&NVIC_InitStruct);
//if i try event_0 with TIM1 upgrade it works event1 is for TIM1_CC4 event
// table 43 reference manual
ADC_InjectedInitStruct.ADC_ExternalTrigInjecConvEvent = ADC_ExternalTrigInjecConvEvent_1;
ADC_InjectedInitStruct.ADC_ExternalTrigInjecEventEdge = ADC_ExternalTrigInjecEventEdge_BothEdge;
ADC_InjectedInitStruct.ADC_InjecSequence1 = ADC_InjectedChannel_1;
ADC_InjectedInitStruct.ADC_NbrOfInjecChannel = 1;
ADC_InjectedInit(ADC1,&ADC_InjectedInitStruct);
ADC_InjectedChannelSampleTimeConfig(ADC1, ADC_InjectedChannel_1, ADC_SampleTime_1Cycles5);
ADC_InjectedDiscModeCmd(ADC1,ENABLE);
ADC_AutoInjectedConvCmd(ADC1,ENABLE);
ADC_StartInjectedConversion(ADC1);
ADC_ITConfig(ADC1,ADC_IT_JEOC,ENABLE);
ADC_Cmd(ADC1,ENABLE);
/* wait for ADRDY */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));
ADC_StartConversion(ADC1);
}
I can see the PWM signal and the upgrade interrupt of TIM1 is working.But i can not enter ADC interrupt if i try to use the code above to trigger ADC Injected interrupt with TIM1 CCR4 event any idea why ?
2018-09-30 6:21 AM
Event 0 is for the TRGO setting, not UPDATE, Event 1 for OC4REF
Code doesn't look unreasonable, would take some debugging to understand the issue. Would probably start by pushing CH4 to a pin in toggle mode, and confirm it is ticking.
I probably wouldn't use the both edges mode, nor TRGO and master/slave settings.
2021-01-09 8:16 AM
Have you slove this?I want to use timer ccr2 event to tirgger the adc,it is fail too.