stm32f3 DISCOVERY ADC DMA INT PROBLEM
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-31 4:51 AM
Posted on October 31, 2014 at 12:51
Hi,
i have a problem with the dma adc conversion, the values ​​of the conversion are correct but the interrupt is called only once. I would like to get an ongoing conversion. main.c
/* Includes ------------------------------------------------------------------*/
#include ''main.h''
#define ADC1_DR_Address ((uint32_t)0x50000040)
#define SIZE 4
#define CHANNEL 4
__IO uint16_t calibration_value = 0;
__IO uint32_t TimingDelay = 0;
bool
flag_ADCDMA_TransferComplete =
false
;
void
Delay(__IO uint32_t nTime);
void
TimingDelay_Decrement(
void
);
void
ADC_Configure(
void
);
__IO uint16_t ADC_Val[4];
uint16_t temp[4];
/**
* @brief Main program.
* @param None
* @retval None
*/
int
main(
void
)
{
RCC_ClocksTypeDef RCC_Clocks;
/* SysTick end of count event each 10ms */
RCC_GetClocksFreq(&RCC_Clocks);
SysTick_Config(RCC_Clocks.HCLK_Frequency / 100);
ADC_Configure();
while
(1)
{
//memcpy(&temp[0],ADC_Val,5);
while
(flag_ADCDMA_TransferComplete ==
false
);
for
(uint8_t i=0; i<4; i++)
{
temp[i]=ADC_Val[i]/4;
}
printf
(
''%d,%d,%d,%d\n\r''
,temp[0],temp[1],temp[2],temp[3]);
flag_ADCDMA_TransferComplete =
false
;
}
}
void
ADC_Configure(
void
)
{
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* GPIOA GIPOF Periph clock enable */
/* Enable ADC1 clock */
/* DMA configuration */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
//------------------------------------------------------------------------
/* Configure ADC Channel7 as analog input */
/* ADC1 per:
* PA1 -> ADC1_IN2
* PA2 -> ADC1_IN3
* PA3 -> ADC1_IN4
* PF4 -> ADC1_IN5
*/
/* PA1 PA2 PA3 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* PF4 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOF, &GPIO_InitStructure);
//------------------------------------------------------------------------
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);
ADC_StructInit(&ADC_InitStructure);
/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC1, ENABLE);
ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC1);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
//
ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;
ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_Circular;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;
ADC_CommonInit(ADC1, &ADC_CommonInitStructure);
while
(ADC_GetCalibrationStatus(ADC1) != RESET );
calibration_value = ADC_GetCalibrationValue(ADC1);
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0;
ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;
ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;
ADC_InitStructure.ADC_NbrOfRegChannel = CHANNEL;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 1,ADC_SampleTime_19Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 2,ADC_SampleTime_19Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_4, 3,ADC_SampleTime_19Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 4,ADC_SampleTime_19Cycles5);
//------------------------------------------------------------------------
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&ADC_Val;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = SIZE;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
// 16 bit
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
// 16 bit
//DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
//------------------------------------------------------------------------
/* Enable DMA1 channel1 IRQ Channel */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Enable DMA1 Channel1 Transfer Complete interrupt */
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
//------------------------------------------------------------------------
// abilita il canale dma per ADC1
DMA_Cmd(DMA1_Channel1, ENABLE);
// abilita adc1 con dma
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* wait for ADRDY */
while
(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));
/* Start ADC1 Software Conversion */
ADC_StartConversion(ADC1);
}
/**
* @brief Inserts a delay time.
* @param nTime: specifies the delay time length, in 10 ms.
* @retval None
*/
void
Delay(__IO uint32_t nTime)
{
TimingDelay = nTime;
while
(TimingDelay != 0);
}
/**
* @brief Decrements the TimingDelay variable.
* @param None
* @retval None
*/
void
TimingDelay_Decrement(
void
)
{
if
(TimingDelay != 0x00)
{
TimingDelay--;
}
}
andstm32f30x_it.c
void
SysTick_Handler(
void
)
{
TimingDelay--;
}
/**
* @brief This function handles DMA Transfer Complete interrupt request.
* @param None
* @retval None
*/
void
DMA1_Channel1_IRQHandler(
void
)
{
DMA_ClearFlag(DMA1_IT_TC1);
flag_ADCDMA_TransferComplete =
true
;
}
#adc #dma #discovery #board #int
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-31 8:13 AM
Posted on October 31, 2014 at 16:13
DMA_ClearFlag(DMA1_IT_TC1);
// wrong function/syntax
void DMA1_Channel1_IRQHandler(void) // 5 Hz
{
/* Test on DMA1 Channel1 Transfer Complete interrupt */
if (DMA_GetITStatus(DMA1_IT_TC1))
{
/* Clear DMA1 Channel1 Transfer Complete pending bit */
DMA_ClearITPendingBit(DMA1_IT_TC1);
STM_EVAL_LEDToggle(LED3); // 2.5 Hz
}
}
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-03 3:07 AM
Posted on November 03, 2014 at 12:07Hi Clive, thanks for the answer, my mistake ...I corrected the routine, but the interrupt is only called once again. I was wrong in some settings?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-01 8:38 PM
Posted on March 02, 2016 at 05:38
I had the same problem of the ADC conversion only happening once. Much digging yielded:
ADC_DMAConfig(ADC1, ADC_DMAMode_Circular); //need this line
I put it right after the ADC_RegularChannelConfig lines