cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3 - AN4296 - ISR FROM CCM RAM USING IAR

Asantos
Senior
Posted on August 20, 2013 at 02:38

Hi,

I would like to receive a working project the demonstrate how to execute an interrupt handler from CCM RAM using EWARM. I tried the procedure from AN4296 section 2.2. The project compiles,  but when the ISR is triggered, the CPU processing get lost.

Ari.
1 REPLY 1
Posted on August 20, 2013 at 03:18

Have you set up the vector table correctly? Is it situated on a 512-byte boundary?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..