2013-06-27 10:52 PM
May I know how can I configure my STM32F205 microcontroler for USART RTS/CTS???
I could not find any resource on the net, and my codes are below but it doesnt work: anyone can help me to configure the CTS/RTS UART configuration thanks!!!// Enable GPIO clock
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOA, ENABLE);
// Enable USART2 clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
GPIO_InitTypeDef GPIO_InitStructure;
// Connect USART pins to AF7
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_USART2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_USART2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);
// Configure USART Tx and Rx as alternate function push-pull
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; //USART Tx
GPIO_Init(GPIOA, &GPIO_InitStructure);
//GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_0;
//GPIO_Init(GPIOA, &GPIO_InitStructure);
//GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
// UART2
NVIC_InitTypeDef NVIC_InitStructure;
// Enable the USARTz Interrupt
NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x4;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
USART_InitTypeDef USART_InitStructure;
USART_StructInit(&USART_InitStructure);
USART_InitStructure.USART_BaudRate = baudrate;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
/* Enable USART2 Receive interrupts */
USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);
/* Enable the USART2 */
USART_Cmd(USART2, ENABLE);
#uart-flow-control #uart.stm32-uart
2013-07-31 04:44 AM
I wanna know it to.
The different in my case is that i am using usart with DMA2013-07-31 05:22 AM
For starters, all the pins should be in AF Mode
If you read the DR, on a RXNE interrupt it's going to re-enable reception, if you don't read DR it will keep re-entering the interrupt handler. If you have buffers behind the USART, you might want to look at handling this manually.2013-09-18 06:36 AM
2013-09-18 07:16 AM
So what's the question here? How do you set up the hardware? or How do you read the bits in the status register and architect that into your buffering scheme?
2013-09-18 11:02 PM
Hello,
Thank you Clive1 for your fast answer. My question is how set up hardware to connect UART6 using RTS/CTS flow control. I have setup as I show below, and I don't receive any data, but I'm sure the other device is sending data: USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* Enable GPIO clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); /* Enable GPIO clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); /* Enable UART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); /* Connect PXx to USARTx_Tx*/ GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6); /* Connect PXx to USARTx_Rx*/ GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6); /* Connect PXx to USARTx_RTS*/ GPIO_PinAFConfig(GPIOG, GPIO_PinSource12, GPIO_AF_USART6); /* Connect PXx to USARTx_CTS*/ GPIO_PinAFConfig(GPIOG, GPIO_PinSource15, GPIO_AF_USART6); // Configure USART Tx as alternate function GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = TX_WIFI; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init (GPIOC, &GPIO_InitStructure); // Configure USART Rx as alternate function GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = RX_WIFI; GPIO_Init (GPIOC, &GPIO_InitStructure); // Configure USART RTS as alternate function GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = RTS_WIFI; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init (GPIOG, &GPIO_InitStructure); // Configure USART CTS as alternate function GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = CTS_WIFI; GPIO_Init (GPIOG, &GPIO_InitStructure); /* USART configuration */ USART_Init (USART6, &USART_InitStructure); /* Enable USART */ USART_Cmd (USART6, ENABLE);I would like to know, what I'm doing wrong.Thank you very much for your helpCarmen2015-09-09 03:43 AM
Hi - why am I getting an overrun error? I am talking to a FT230 chips with cts/rts handshaking. Why is the cts/rts obviously not working? It is running in main()
//STM32F303x
void setupUART2( void )
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
USART_StructInit(&USART_InitStructure);
USART_DeInit(USART2);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_7); //CTS
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_7); //RTS
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7); //Tx
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7); //Rx
//Configure USART2 pins:
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 57600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2,ENABLE);
}
char readUSART( void )
{
FlagStatus flagRXNE = RESET; //Receive data register not empty flag
char data=0;
flagRXNE = USART_GetFlagStatus(USART2, USART_FLAG_RXNE);
if (flagRXNE == SET)
{
data = USART_ReceiveData(USART2); //A read clears flagRXNE
}
else
{
data = 0;
}
if (USART_GetFlagStatus(USART2, USART_FLAG_ORE)==SET) ledOnOff( LED_10, ON );
if (data !=0) stringToUSART( &data, 1 ); //Echo test
return( data );
}
2015-09-09 05:20 AM
I think you'd need to stick the pins on a logic analyzer to understand what the interaction is. Confirm the FT230 actually stops sending when requested to do so.
2015-09-09 06:48 AM
It seems that I set RTS inactive high at the end of the first Rx byte, but then the FT230 sends me 2 bytes more before stopping. Going to have to take this up with them, because if it is the default behaviour it's serious
BTW, this site is seriously flaky. My real name is Dirk Bruere but I could not sign in under it and could not follow any recovery procedure2015-09-09 08:59 AM
It's some hunk of junk from Microsoft, I've got a dead account here because the system uses an email id, and you can't change the email address, because who ever does that? It's about the most brain damaged forum software ever, and it's not like Microsoft didn't have access to two decades worth of working examples of how to do it properly... I'm so glad they've got so totally killed in the mobile space.
Yeah, I don't think FTDI is going to fix their silicon, any more than I think ST will. The 1-byte deep design is just lazy, and if you're going to put a deeper buffer behind it, and who wouldn't, I'd just manage the flow control there, where you have some margin and some control.