2023-07-13 3:18 AM - edited 2023-07-13 3:20 AM
Hi Mr. and Miss.
At present, I use a circuit board designed by myself, using STM32F207VGT6. Initialize the VCP function using STM32CubeIDE. But there was a phenomenon that it couldn't solve. Error Code10 displayed on Windows.
Attached is my circuit diagram and the settings of CubeIDE(Only initial setting without any code add or modified)
Where would this be causing the problem? Please give me some advice, much thanks.
2023-07-20 12:02 PM - edited 2023-07-20 12:03 PM
Update Windows Forms 10 to 11.
https://en.wikipedia.org/wiki/Windows_Forms
Less nonsense would help... And the proper solution is tossing out the broken bloatware and using, for example, this: