2013-04-24 2:19 AM
Hi,
I'm looking to sample a signal (well, 2 actually - quadrature analog signals) at a fixed sample rate, but I'm baffled by the lack of any example in the Standard Peripheral Library on how to achieve this.I would have thought that this would be a pretty standard example, i.e sample x points of a signal at y kHz and store result in memory location z.Can anyone from ST comment on why such a basic (and imo fundamental) example is missing from the Standard Peripheral Library?Does anybody else have an basic example of how this is achieved? There are various incomplete snippets of code if you search in this forum, but elsewhere on the internet I've been able to find zilch.I suspect I'm going to have to go read the manual in depth to figure this lot out...oh joy!Many thanks.Adrian2015-08-30 7:38 AM
It should decimate. Pairs of samples, interrupting halfway through as it fills each half.
So 800 sample buffer / (2 * 2) = 200 sample pairs between interrupts200 KHz / 200 sample periods = 1 KHz2015-11-13 9:40 AM
Hi!
I wrote code, but it stuck inADC_GetStatus(ADC1). Could someone help me? ________________ Attachments : adc.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0q9&d=%2Fa%2F0X0000000beJ%2FlEMPW7LxCO96c_2NpElozBrofR_TW_hlu6ofZ5JejGA&asPdf=false2015-11-13 9:42 AM
Problem, I stuck in ADC_GetStatus(ADC1).
#include <stm32l/rcc.h>#include <stm32l/nvic.h>#include <stm32l/gpio.h>#include <stm32l/stm32l.h>#include <stm32l/exti.h>#include <stm32l/syscfg.h>#include <stm32l/adc.h>#define BUFFERSIZE 1000 /**************************************************************************************/void simple_delay(uint32_t us){ /* simple delay loop */ while (us--) { asm volatile (''nop''); }} void RCC_Configuration(void){ RCC_AHBPeriphClockCmd(AHB_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(APB2_ADC1, ENABLE); RCC_AHBPeriphClockCmd(AHB_GPIOB, ENABLE);} /**************************************************************************************/ void GPIO_Configuration(void){ /* ADC Channel 2 -> PA2 */ gpio_init_t gpio; GPIO_StructInit(&gpio); gpio.pins = GPIO_P2; //pin A2 gpio.mode = GPIO_ANALOG; //analog gpio.pupd = GPIO_P_NOPULL; // no pull /* apply configuration */ GPIO_Init(GPIOA, &gpio); gpio_init_t gpio1; GPIO_StructInit(&gpio1); gpio1.pins = GPIO_P7; gpio1.mode = GPIO_OUTPUT; gpio1.otype = GPIO_OT_PP; GPIO_Init(GPIOB, &gpio1); } /**************************************************************************************/ void ADC_Configuration(void){ adc_init_t adc; adc_init_com_t adc_com; ADC_CommonStructInit(&adc_com); ADC_StructInit(&adc); /* ADC Common Init */ adc_com.prescaler=ADC_PRESCALER_DIV4; ADC_CommonInit(&adc_com); adc.resolution = ADC_RESOLUTION_12b; adc.scan_conv_mode = DISABLE; // 1 Channel adc.continuous_conv_mode = DISABLE; // Conversions Triggered adc.external_trig_conv_edge = ADC_EXTTRIGCONVEDGE_RISING; // Manual adc.external_trig_conv = ADC_EXTTRIGCONV_T2_TRGO; adc.data_align = ADC_DATAALIGN_RIGHT; adc.conversion_num = 1; ADC_Init(ADC1,&adc); /* ADC1 regular channel 11 configuration */ ADC_RegularChannelConfig(ADC1, ADC_C2, 1, ADC_SAMPLETIME_4C); // PC1 /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE);} // blinking void led_blink(){ GPIO_SetPins(GPIOB, GPIO_P7); /* delay */ simple_delay(100000); /* clear led */ GPIO_ClearPins(GPIOB, GPIO_P7); /* delay */ simple_delay(100000);} /**************************************************************************************/ uint16_t ADCConvertedValues[BUFFERSIZE];uint32_t ADCStat = 0x0; int main(void){ uint16_t reg; int i; RCC_DeInit(); RCC_Configuration(); GPIO_Configuration(); ADC_Configuration(); i = 0; GPIO_SetPins(GPIOB, GPIO_P7); simple_delay(1000000); GPIO_ClearPins(GPIOB, GPIO_P7); simple_delay(1000000); ADC_SoftwareStartConv(ADC1); if(ADC_GetSoftwareStartConvStatus(ADC1)){ GPIO_SetPins(GPIOB, GPIO_P7); } while((ADC_GetStatus(ADC1)&0x2)==0); GPIO_ClearPins(GPIOB, GPIO_P7); ADCConvertedValues[i++] = ADC_GetConversionValue(ADC1); i %= BUFFERSIZE; while(1) // Don't want to exit { }}2015-11-13 10:55 AM
When you are using an STM32 part that's unrelated to the thread's stated topic please open a new thread about your question and problem.
I'm not familiar with the library you are using, it seems to be a mix of SPL with something else. Please state clearly what you're using. The L1 needs the HSI clock enabled for the ADC to function./* Enable The HSI (16Mhz) */
RCC_HSICmd(ENABLE);
/* Check that HSI oscillator is ready */
while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET);
2015-11-13 10:59 AM
This first one is an on-topic, on-point thread
https://community.st.com/0D50X00009XkiMhSAJ
Edit: Fixed DEAD LINKs