cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F205RG RTC Problem.

Greetings,

I have connected external crystal of 32.768 KHz to STM32F205RG for RTC time keeping purpose. I have also enabled RTC output on pin PC13. Below is my code for RTC Initialization ...

int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_RTC_Init(); if (HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2) { /* Configure RTC Calendar */ RTC_CalendarConfig(); } else { /* Check if the Power On Reset flag is set */ if (__HAL_RCC_GET_FLAG(RCC_FLAG_PORRST) != RESET) { } /* Check if Pin Reset flag is set */ if (__HAL_RCC_GET_FLAG(RCC_FLAG_PINRST) != RESET) { } /* Clear source Reset Flag */ __HAL_RCC_CLEAR_RESET_FLAGS(); } /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { RTC_CalendarShow(aShowTime, aShowDate); if(_set) { RTC_CalendarConfig(); _set = 0; } } /* USER CODE END 3 */ }
View more

This is the main code and code for RTC_CalendarShow and RTC_CalendarConfig is as below

static void RTC_CalendarConfig(void) { if(HAL_RTC_SetDate(&hrtc,&sDate,RTC_FORMAT_BCD) != HAL_OK) { /* Initialization Error */ Error_Handler(); } if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK) { /* Initialization Error */ Error_Handler(); } /*##-3- Writes a data in a RTC Backup data Register1 #######################*/ HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR1, 0x32F2); } static void RTC_CalendarShow(uint8_t *showtime, uint8_t *showdate) { RTC_DateTypeDef sdatestructureget; RTC_TimeTypeDef stimestructureget; /* Get the RTC current Time */ HAL_RTC_GetTime(&hrtc, &stimestructureget, RTC_FORMAT_BIN); /* Get the RTC current Date */ HAL_RTC_GetDate(&hrtc, &sdatestructureget, RTC_FORMAT_BIN); /* Display time Format : hh:mm:ss */ sprintf((char *)showtime, "%2d:%2d:%2d", stimestructureget.Hours, stimestructureget.Minutes, stimestructureget.Seconds); /* Display date Format : mm-dd-yy */ sprintf((char *)showdate, "%2d-%2d-%2d", sdatestructureget.Date, sdatestructureget.Month, 2000 + sdatestructureget.Year); }
View more

The problem is after like 4 hours of run rtc is ahead approx 2 seconds or more. How to solve this problem ? 

The calibration output on pin PC13 gives me perfect 512 Hz wave as i have verified on oscilloscope. The same code is running prefectly fine on NUCLEO-F207ZG board.

2 REPLIES 2

Sorry didn't see any initialization code, need to have different prescalers for LSI vs LSE.

Need to use 6-7pF crystals on the F2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Greetings Tesla,

I have used cube for code initialization. I am attaching the screen shots of the cube for better understanding.Screen 1.pngScreen 2.pngScreen 3.png