STM32F1Cube drivers bug
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-16 3:25 AM
Dear,
I am currently using the STM32F1Cube drivers on a STM32F107VC MCU (STM3210C-EVAL board) and I discovered a bug in CAN drivers.
The problem is in the 'stm32f1xx_hal_can.h file on line 379.
#define CAN_FLAG_TXOK2 ((uint32_t)((TSR_REGISTER_INDEX << 8U) | CAN_TSR_RQCP0_BIT_POSITION)) /*!< Transmission OK MailBox2 flag */
When you send a CAN frame, the IRQ (HAL_CAN_IRQHandler) always call CAN_Transmit_IT/HAL_CAN_TxCpltCallback even if the transmission failed. Your never have 'HAL_CAN_ERROR_TXFAIL' as error code.
If you have a CAN configuration with no automatic retransmission without other device connected on bus CAN and you try to send a CAN frame you never know than you have a transmission error.
This must be
#define CAN_FLAG_TXOK2 ((uint32_t)((TSR_REGISTER_INDEX << 8U) | CAN_TSR_TXOK2_BIT_POSITION)) /*!< Transmission OK MailBox2 flag */
I don' know if it's the good place to report this bug.
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-16 3:40 AM
Hello
DANNEL.Yannick
,Thank you for your reported issue.
This wrong define for CAN_FLAG_TXOK2 is confirmed and raised internally to the appropriate team for fix in the coming release.
Best Regards,
Imen.
Thanks
Imen