2014-03-14 8:02 AM
1. Everything normal
2014-03-14 8:11 AM
Based on your addresses the stack is pitifully small for the allocations you are making.
Make the stack bigger, perhaps in your linker script or startup file, you don't mention a tool chain, and I'm not going to guess.2014-03-14 8:22 AM
Thanks for the reply!
I'm on CooCox CoIDE v.1.7.6 with arm-none-eabi-gcc 4.8 2013q4.The linker setup seems correct to me though:2014-03-14 8:37 AM
You are describing the size of the RAM, not the SIZE and PLACEMENT of the STACK within that space.
In Keil we define the stack within startup_stm32f1xx_xx.s, where you'd do it the the CooCox GUI I don't know. For GNU/GCC it is often defined in the linker script, points to the top of memory and moves down to the heap. You appear to be defining a stack in the 512 byte range, and it's placed very low in RAM. If CooCox doesn't have documentation, or you can't find it in your GUI, try their forum.2014-03-14 8:41 AM
Look (search/grep) your project files for something like this..
#define STACK_SIZE 0x00000200
__attribute__ ((section(''.co_stack'')))
unsigned long pulStack[STACK_SIZE];
2014-03-14 9:05 AM
Found it!
.\cmsis_boot\startup\startup_stm32f10x_md.c I entered/*----------Stack Configuration-----------------------------------------------*/
#define STACK_SIZE 0x00001000 /*!< The Stack size suggest using even number */
__attribute__ ((section(''.co_stack'')))
unsigned long pulStack[STACK_SIZE];
What I dont get: why does
#define STACK_SIZE 0x00000100
increase
bss to 1024
? (0x400) Do I need the heap (when programming in (static) C, so nonew
ormalloc
) at all?2014-03-14 9:42 AM
I don't know, what else is in your project?
Can you review the .MAP output by the linker to determine the memory use/foot-print? If none of you code, or libraries, uses malloc()/new, then the heap can be small. You might be able to eliminate it, depends on what other code expects to support it, etc.2014-03-14 10:39 AM
What else is in my project? Nothing:
int main(void)
{
while(1)
{
}
}
I'm only fooling around with the stack size... Mapfile for stacksize0x00000200 is attached. excerpt from map-file (0x200, bss=2048): .heap 0x20000000 0x0
0x20000000 __end__ = .
0x20000000 _end = __end__
0x20000000 end = __end__
*(.heap*)
0x20000000 __HeapLimit = .
.co_stack 0x20000000 0x800
0x20000000 . = ALIGN (0x8)
*(.co_stack .co_stack.*)
.co_stack 0x20000000 0x800 ..\obj\startup_stm32f10x_md.o
0x20000000 pulStack
0x20005000 __StackTop = (ORIGIN (ram) + 0x5000)
0x20004800 __StackLimit = (__StackTop - SIZEOF (.co_stack))
0x20005000 PROVIDE (__stack, __StackTop)
0x00000001 ASSERT ((__StackLimit >= __HeapLimit), region ram overflowed with stack)
excerpt from map-file (0x100, bss=1024): .heap 0x20000000 0x0
0x20000000 __end__ = .
0x20000000 _end = __end__
0x20000000 end = __end__
*(.heap*)
0x20000000 __HeapLimit = .
.co_stack 0x20000000 0x400
0x20000000 . = ALIGN (0x8)
*(.co_stack .co_stack.*)
.co_stack 0x20000000 0x400 ..\obj\startup_stm32f10x_md.o
0x20000000 pulStack
0x20005000 __StackTop = (ORIGIN (ram) + 0x5000)
0x20004c00 __StackLimit = (__StackTop - SIZEOF (.co_stack))
0x20005000 PROVIDE (__stack, __StackTop)
0x00000001 ASSERT ((__StackLimit >= __HeapLimit), region ram overflowed with stack)
.co_stack seems to be always 4 times larger than STACK_SIZE...
________________
Attachments : StructTest.map : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0r3&d=%2Fa%2F0X0000000beV%2F_2Ecr7EN_hZWO8b9pmQeOxf9RzGAJlYetwKBGZB6wtc&asPdf=false
2014-03-14 10:52 AM
.co_stack seems to be always 4 times larger than STACK_SIZE...
No doubt because it's defined as an array of ''unsigned long''s which are 32-bit wide.2014-03-15 1:59 AM
To be honest, you really shouldn't be allocating variables as large as that on the stack. The total size of those is going to be several kilobytes!
Prefixing them with the ''static'' keyword will move them to the heap, but bear in mind they'll keep their value through successive runs of the function. That is to say, if function ''foo'' has a static int which it sets to 123, when it's run again, that value will be pre-set to ''123'' again. As a bonus, the linker will complain if you try to allocate more variables than you have available heap memory.